LSM330TR: Reading Accelerometer Output
Posted on October 27, 2016 at 11:00The original post was too long to process during our migration. Please click on the attachment to read the original post.
Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Posted on October 27, 2016 at 11:00The original post was too long to process during our migration. Please click on the attachment to read the original post.
Posted on October 27, 2016 at 08:56Hai,I am sathish from Comtustec India Pvt., LTD., Coimbatore, In my design I am using your LIS2DS12.Can you please provide me a footprint and step file of that sensor.
Posted on September 29, 2016 at 21:04When the force sensor is powered off the LSM is always on and the microcontroller is in sleep mode. Sometimes the battery will drain to empty. When powered back up the LSM gets hot although it still works. We ...
Posted on October 26, 2016 at 17:36I'm using a STEVAL-IME002V2 single lead ECG evaluation board. I do not use the ECG DB 15 connector, instead i make use of the RL,LA and RA leads in the board to connect the electrodes. I'm trying to get the heartb...
Posted on October 26, 2016 at 17:33I'm using a STEVAL-IME002V2(HM301D) single lead ECG evaluation board. I do not use the ECG DB 15 connector, instead i make use of the RL,LA and RA leads in the board to connect the electrodes. I'm trying to get th...
Posted on October 25, 2016 at 17:01We are using the LSM9DS0TR and here is what I am seeing� I have both CS-G and CS_XM tied t0 3.3V and SDDO_G/SAO_G and SDO_XM/SAO_XM tied to GND, this should give me the following I2C addresses (we are using I2C t...
Posted on September 26, 2016 at 14:54Hi Team , We are working on LIS2DH12 chip for accelerometer and temperature readings . Hardware Cicuit details : a. VDD and VDDIO : 1.8 V We are facing issue in the temperature readings. Please find below for the...
Posted on October 19, 2016 at 17:30 Hello, I have a problem with the LIS331HH Sensor. The X and Y direction are send correctly to my microcontroller, only the Z value has an offset. I've tried different LIS331HH and the offset is no...
Posted on October 25, 2016 at 12:01Hi,I am trying to find MEMS wireless accelerometer. It can be an integrated device or a small board. Does ST has one ? Thanks for the help. #mems #accelerometer #wireless
Posted on October 21, 2016 at 14:30 Hello, Recently I've been tasked with modifying existing code running on a system which contains a LIS2DH accelerometer. It should be pointed out that I'm used to high-level programming languages and th...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.