L3G4200D unacceptable big values WHY?
Posted on October 04, 2016 at 13:36The original post was too long to process during our migration. Please click on the attachment to read the original post.
Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Posted on October 04, 2016 at 13:36The original post was too long to process during our migration. Please click on the attachment to read the original post.
Posted on October 05, 2016 at 10:46I want to use my STM32F429 Discovery's on board L3GD20 to measure an angle from the horizontal, so I only need one axis. I am able to read the acceleration data but I am unsure about a few things: 1. What do I do w...
Posted on November 13, 2016 at 08:16Hi, i need a project HAL STM32 + MPU-6050. Recently, start learning, still very difficult... #mpu6050
Posted on August 19, 2016 at 06:37Hello, We are working on 9 Axis Sensor : LSM9DS0 which is interfaced with MCU over I2C interface. Please find the attached circuit diagram for your reference. Also, We have checked using evaluation board (STEVAL-MKI...
Posted on November 16, 2016 at 17:25Which flux is best for attachment of this product? Is this device susceptible to damage if cleaned using an aqueous wash?
Posted on November 07, 2016 at 06:47We need it to run one signal integrity simulation. Thanks!
Posted on November 02, 2016 at 15:27Hello!Im working with the LSM9DS0 and would like to get further Information about the used Magnetometer.Is there a way to get information about the Hysteresis, Linearity and Repeatibility Error in %FS (or mGauss) ...
Posted on March 16, 2015 at 07:14At work I am using the LIS3DH accelerometer to detect body motion. It is configured for +/-2 gs, 50 samples per second, with Streaming FIFO. The watermark works fine for determining when the FIFO needs to be emptie...
Posted on November 09, 2016 at 07:32I am using LIS332AR mems chip for vibration measurement. Assembled this chip in PCB and PCB located vertical with respect to ground. For every 90 degree rotation of this chip corresponding X and Y axis value chang...
Posted on November 09, 2016 at 07:36Guys, We need to detect vibration as well as tilt. Is there any ready made module available for this application. or any chip available?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.