MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM303D Interrupt

Posted on December 01, 2016 at 12:40I am having trouble getting the click interrupts to work for the LSM303D. using the library provided by Pololu for arduino I can get this code working for the DLHC[code]#include <Wire.h>#include <LSM303.h>long thi...

MP34DT01 sensitivity for far-field application

Posted on October 06, 2014 at 20:30Hello, I would like to prototype a conference room microphone. Is the MP34DT01 mic able to capture sound from a human speaker away from 3 or 4 meters ? (ex: classroom) If no, what would be the recommended mic ? In ...

pierre by Associate
  • 1331 Views
  • 1 replies
  • 0 kudos

Resolved! How to configure LIS2DE12 to support ODR=5.3kHz ?

Posted on December 13, 2016 at 01:06Hi All, I am developing device to analyze vibration with LIS2DE12 acceclerometer.I have encountered problem that sensor did not work with ORD=5.3kHz, it worked fine for all other ODRs.How to configure sensor to wo...

q.lsm6ds3 anti-aliasing filter order

Posted on May 09, 2016 at 13:05hi, I've got a few questions. 1. what is the order anti-aliasing filter of the Acc? 2. what is the order anti-aliasing filter of the Gyro? 3. how does the DLPF1 filter help me if the cut-off freq is higher then nyquist...

amir5 by Associate
  • 1958 Views
  • 3 replies
  • 0 kudos

FIFO alignment is not correct after some time

Posted on September 26, 2016 at 23:15We enabled GyroScope and acclerometer. We set FIFO Mode to continuous with BDU bit is set. We set ODR rate to 1.66kHz . We are reading FIFO continuously. we are observing FIFO data mis-alignment Can somebody help...

Unexpected current consumption from LSM303D

Posted on February 04, 2017 at 03:36Hi,   We are developing a ultra low power sensor module with the LSM303D. The LSM303D was periodically waken up to take a  magnetic and temperature measure (no acceleration measurment). The total excepted average ...

0690X00000603MmQAI.jpg
looeyc by Associate II
  • 1226 Views
  • 1 replies
  • 0 kudos

LSM9DS0 Accelerometer noise

Posted on January 17, 2017 at 19:16Hi.I am using the LSM9DS0, and have observed a lot of noise on the z-Axis of the Accelerometer Data. The attached picture is a plot showing the noise while operating at 100Hz in the +-2g range. Is this a normal lev...

0690X000006064IQAQ.png

LSM303D // Compass X,Y & Z's MSB locked

Posted on March 26, 2015 at 14:53 Hey there, I recently installed a new LSM303D (accelerometer + compass) on my board and I am having some issues with it. I can read the data from the accelerometer fine, but the ones from the compass seem...

STEVAL WESU1 understanding logged data

Posted on October 26, 2016 at 16:43Hi , I have STEVAL WESU module  and logged acelerometer data using android app. (plz see attached file)My settings are: Timer: 512 Hz, 10Hz, 1HzMEMS Accelerometer output data rate: 416 Hz , 833 Hz, 100HzIn the logg...

abhi1new by Associate
  • 1773 Views
  • 2 replies
  • 0 kudos

Reading status register of LSM6DS3

Posted on January 31, 2017 at 06:12hi,     I am Reading the Accelerometer and Gyroscope sensor values by checking the XLDA and GDA bits as follows             if((readReg(STATUS_REG)&0x01)==0x01)     // checking XLDA        {              Ax = (int1...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.