MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LSM6ds3tr Pin Connection with Microcontroller

Hello To receive various Interrupt events how INT1 and INT2 Pins of LSM6ds3tr need to be connected with Microcontroller ?My assumption is INT1 and INT2 pins need to be connected with microcontroller GPIO pins and GPIO pins has to be configured to cat...

Ajit1 by Associate
  • 907 Views
  • 1 replies
  • 0 kudos

How to calculate dBSPL from sound level

Hello all,I have a question regarding the MEMS audio sensor MP23DB01HP. I managed to read out the Soundlevel of the sensor. But I don't know how to interpret this value. My question is, how can I convert the soundlevel to obtain a corresponding value...

riyolu by Associate
  • 3393 Views
  • 4 replies
  • 0 kudos

LSM303AGRTR

With LSM303AGR to achieve the electronic compass function now 0-360 degrees can be obtained normally, has increased the calibration function; Why the uneven distribution 

leo12345678_0-1739840880586.png

LSM6DSV half precision error at ~180 degrees

Hi,We're using the lsm6dsv's SFLP algorithm to calculate IMU rotation. Recently however we noticed that the resulting rotation has big gaps at around the 180degree mark. We believe this is because of the half float precision, specifically because the...

1000000957.png
Gorbit99 by Associate III
  • 18658 Views
  • 29 replies
  • 15 kudos

Unable to calibrate LPS22DF

I am using a python script to update the One Point Calibaration register 1Ah, 1Bh. I put values in but the resultant reading of the normal pressure registers in 28h, 29h, 2Ah are way off. Does anyone have a script that might show exactly how it is do...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.