2025-02-19 2:58 AM
Hello
To receive various Interrupt events how INT1 and INT2 Pins of LSM6ds3tr need to be connected with Microcontroller ?
My assumption is INT1 and INT2 pins need to be connected with microcontroller GPIO pins and GPIO pins has to be configured to catch IMU Interrupt events. Please Support whether this assumption is correct or not.
Solved! Go to Solution.
2025-02-20 2:20 AM
Welcome @Ajit1, to the community!
Yes, your assumption is correct: in order to trigger an interrupt, INT1 and/or INT2 must be connected to interrupt-capable GPIOs.
Regards
/Peter
2025-02-20 2:20 AM
Welcome @Ajit1, to the community!
Yes, your assumption is correct: in order to trigger an interrupt, INT1 and/or INT2 must be connected to interrupt-capable GPIOs.
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.