MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM6DS3US SPI interface

Posted on June 28, 2018 at 14:48I plan on using the LSM6DS3US with an SPI interface. To do this i have to set the CS line to 1. The SPI bus I have is a shared bus with SPI memory devices, each controlled by their own CS line. Therefore on first glan...

bi direction communication on Bluetooth

Posted on June 29, 2018 at 11:58Hi Have anyone tried the full-duplex communication on BlueNRG -2 module for mobile communication? It does not detect as an audio device, it simply shows Bluetooth device. if anyone did so please guide us.Thanks in adv...

VL53L0X Register Map

Posted on February 17, 2017 at 20:28I've been trying to use the VL53L0X TOF sensor to get ranging data but I'm having trouble finding what all the registers do? I tried looking through the datasheet and API specs but nothing seemed to clearly tell m...

A3G4250D gyro measurements

Posted on November 05, 2012 at 18:57I cannot find a forum for MEMS sensors, so I'm posting here. Is anyone using the a3g4250d gyro?  I'm having a problem where I get only one set of measurements after power up.  After that, the measurements do not c...

VL53L1X Issue

Posted on June 28, 2018 at 09:00HiI am facing issue while taking multiple readings for averaging in the VL53L1X sensor.Our sensor is interfaced with B-L072Z-LRWAN1.We are not getting consitent reading as shown below:2486249024892490248724882490Above...

l3gd20h self-test limits?

Posted on March 18, 2016 at 14:09Hi, Which limits should check against when enabling the l3gd20h self-test functionality? Regards,

LSM303AGR and int1

Posted on June 27, 2018 at 11:09With the next configuration, the INT1 don't start.Base on (https://github.com/STMicroelectronics/STMems_Standard_C_drivers/tree/master/lsm303agr_STdC)lsm303agr_xl_operating_mode_set(&dev_ctx_xl, LSM303AGR_XL_POWER_DOW...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.