Resolved! L3GD20H raw value conversion
How does one convert:Raw angular rotation data to DPSRaw temperature sensor readings to degreesThanks :grinning_face:
Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
How does one convert:Raw angular rotation data to DPSRaw temperature sensor readings to degreesThanks :grinning_face:
In CubeMX the HTS221 driver was chosen.While looking to use the sensor within the code, i can't find any documentation how to initialize the sensor.In the HTS221 headerfile i can find: HTS221_Init(HTS221_Object_t *pObj)This function uses a HTS221_Obj...
Dear support,I'm looking for an accelerometer and the one we work with is normally LIS2DE12, but I think it does not work for the product I'm looking for.In the INT1_SCR register, high and low interruption events can be enabled in the different axes,...
When we applied moisture-proof coating to the substrate, we also coated the LPS22HB.In this case, does the coating affect the measurement?If so, is it okay to rub the sensing area to remove the coating?
Is the accelerometer temperature output in OUT_ADC3 still 8 bits if the LPen bit in CTRL_REG1 is cleared?If that is the case, does the temperature change with one digit in OUT_ADC3_H per °C?
I have enabled 2 interrupts on the LIS3DH all on the I2C Bus :1) Data Ready Interrupt 2) Orientation Change InterruptBut during runtime only the Data Ready Interrupt is working. While reading the INT1_SRC register no value is generated. Even after di...
I need to connect Microphone to BlueNRG-2 and How Can I interface with the Chip.?
We understood the ODR and correlated filtering. A following micro-controller application performs further filtering with averaging values to 10 per second. Aimed is calculating an angle derived from the rotational speed. Precision should be about or ...
Hi!We configured it fifo contineous mode to further reduce the current consumption of the lsm6dsl mounted on our own board with nRF52832(nordic semiconductor), but rather the current consumption has increased. Total current consumption has increased ...
Hi,I have a MKI109V3 and one MKI197V1.I have downloaded the related tools&software of MKI109V3 then I opened the DfuSe Demo from en.stsw-mki109w / MEMS_Demonstration_Kit_SW_package_v8_0_WINDOWS and upgraded ProfiMEMSToolV2.40.1.dfu from ProfiMEMSTool...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.