Resolved! Current consumption enabling FSM on LSM6DSOX
Hi, how much is the additional current consumption enabling the FSM on LSM6DSOX? Regards
Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Hi, how much is the additional current consumption enabling the FSM on LSM6DSOX? Regards
On a workshop I heard of this. For an application I would need a bit more precision especially in gyro resolution / stability. Can you please send me information on this and the MEMS identifier, eg ISM330HLC or ISM330DHC ... Are samples available, e....
I'm setting up LIS2DW12 to 100Hz, low power mode 1, fifo threshold 30 and fifo interrupt on INT2.When interrupt is received by MCU (STM32L4 here) i readout register 0x2F to know how much samples is to retrieve, then retrieve them all by issuing read ...
I would like to use the VL53L0X in a 3D printed tube with limited space. The diameter is 6,5mm.Since the emitter and collector have a conical characteristic, there are limitations as describes in an earlier post: https://community.st.com/s/question/0...
Hi,I'm working with a STM32F401 Nucleo-64 board. The board is connected to a mems accelerometer (IIS2DH) via SPI, and I'm using the HAL library.Everything was working good and I was able to retrieve samples from the accelerometer. Suddenly one day la...
Posted on June 19, 2017 at 20:00We're using the LIS2HH12 accelerometer and there's a temperature sensor listed in the datasheet accessible via the temp_L and temp_H registers (16 bits).However the numbers I get don't make any sense.The datasheet men...
I'm new to Accelerometer Sensor.I have few questions o this LIS2DH12TR.There are two Interrupt pins on this LIS2DH12TR.The interrupt pins are meant for Threshold detection and sending the LIS2DH12TR to sleep/wakeup mode? Can you briefly explain the f...
Hello, I need help using L3GD20 gyroscope that comes with stm32f429ZI DISC! board. I have used code in this thread as the example and this video to generate code using cube MX/* Includes ---------------------------------------------------------------...
Recovery of Standby Mode in LIS3DH + STM32L072I am developing using LIS3DH + STM32L072 now.I think that I want to restore with WKUP (PA0) of STM32L072 by INT1 when it enters Standby Mode and exceeds the threshold set to LIS3DH.However, I will not ret...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.