MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STEVAL-BCN002V1 Sensor Demo Project Code Walk-through

STEVAL-BCN002V1 Sensor Demo Project Code Walk-throughDear all, I am new to STEVAL-BCN002V1.I will like to inquire if there is any workshop presentation materials or materials which can explain to me the code walk-through for the entire STEVAL-BCN002V...

garyng98 by Associate
  • 1095 Views
  • 1 replies
  • 0 kudos

LIS3DHH interrupt always high

Hello, I've successfully initialized LIS3DHH on STEVAL_MKI180V1 board and been reading values from it. I've also enabled the interrupts but they always seem high (I've added a LED to the INT1 line). What I'd like to do is some threshold on movement, ...

AChri.15 by Associate
  • 1007 Views
  • 1 replies
  • 0 kudos

Power supply of LSM303AH

Hello,I am using steval-miki173v1 for testing LSM303AH.I have supplied this one by mistakes with 3.3v. And its working well, but not good idea sure.I have made the same mistakes on my customized PCB, supplied LSM303AH directly with 3.3 and this is do...

rimbaud by Associate II
  • 1210 Views
  • 2 replies
  • 0 kudos

LIS3DSH Intermittent X,Y,Z Readings

I can write and read back all registers so everything seems to be fine with the SPI communications but I keep getting very odd readings on X, Y, and Z OUT registers. I'm following the simple setup in the application note, CTRL_REG4 = 0x67 and CTRL_RE...

Gacekky by Associate
  • 1431 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.