MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

BlueNRG-232 tile won't enable

I've had intermittent success at flashing the firmware provided with the DK for the BlueNRG tile (STEVAL-BCN002V1) when attached to the host board. I can see the image file loading on to the device memory followed by a successful verify and sometime...

RGupp by Associate II
  • 1513 Views
  • 2 replies
  • 0 kudos

How to use SHT21 humidty sensor with i2c2 on STM32F103?

Hello everyone,I want to receive humidty from SHT21 sensor. I received first or a few data and then this communication stop. Why? Can you help me please ?http://www.farnell.com/datasheets/1780639.pdf this is datasheet of SHT21Thank you

A3G4250D: convert OUT_TEMP value to actual tempera

I am using A3G4250D gyroscope in one of our project. I want to know how to convert RAW value read from register OUT_TEMP (26h) to actual temperature values? I know that OUT_TEMP register in two’s complement format with a sensitivity of -1 LSB/°C but ...

DS by Associate
  • 1238 Views
  • 1 replies
  • 0 kudos

Resolved! Setting a threshold value

Hi ,i need to know how to set a threshold value for state machine interrupt, can u explain with an example. precisely means setting the value in the register for wakeup statemachine

MKS by Associate II
  • 2779 Views
  • 5 replies
  • 0 kudos

How can I reduce the influence of sunlight with the ToF VL53L1X

For my application I use the ToF VL53L1X.I need to measure the distance from 10cm to 1m in front on a plate surface.I have done some characterisations on a distance test bench indoor, and I have obtained good results.For my application I have to use ...

BMith by Associate
  • 1997 Views
  • 1 replies
  • 0 kudos

Problems with Getting Started Application b/w X-NUCLEO-GNSS and B-L475e-IOT01A1. No previous connection to the Internet is done by the B-L475e-IoT node.

The guide/documentation provided talks mainly b/w the X-NUCLEO-GNSS sensor and a NUCLEO board while I am attempting to use the L475e-IoT Node. When interacting with the application on Tera Term, the menu from the example is displayed. However, when a...

MChav.13 by Associate II
  • 1704 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.