2019-07-10 7:59 PM
STEVAL-BCN002V1 Sensor Demo Project Code Walk-through
Dear all, I am new to STEVAL-BCN002V1.
I will like to inquire if there is any workshop presentation materials or materials which can explain to me the code walk-through for the entire STEVAL-BCN002V1.
As I will only use acclerometer and pressure sensor to get free-fall function, step counter, acitivites recongition.
Also, I will like to ask why am I able to add the customised C code which I had build using algobuilder to the whole project.
Please teach.
Best Regards
Gary
2019-07-15 7:54 AM
Hi @garyng98 , please consider that the STEVAL-BCN002V1 is based on the X-CUBE-MEMS1 firmware library package. To be more specific, the mid-level code function explanation can be found in the proper User manuals, such as:
Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.