2020-01-10 9:57 AM
I have 2 LSM9DS1 9 axis chips and after waving them around I have the following min / max magnetometer values:
chip1:
X max/min: 657/-396
Y max/min: 598/-417
Z max/min: 377/-654
chip2:
X max/min: 533 -515
Y max/min: 788/-284
Z max/min: 0/-1213
...that last Z max/min on chip2 looks bad. How does it look to others? Are these chips (roughly) calibrated at the factory? Is there a setting inside the chip that can fix this - if it is a problem?
-thanks
2020-01-10 9:59 AM
Oh, just had a thought! What if chip 2's Z magnetometer was never larger than zero? I bet my code doesn't account for a negative "max" value. But still, isn't that really far off from what these LSMDS1 magnetometer chips should be reporting for a maximum?
2020-01-10 1:54 PM
So, I am looking for very low or negative maximum values from the Z axis magnetometer for my chip 2 (an STMicro LSM9DS1) and got the following average maximum: (-203.667) and the following average minimum: (-1182.67). If I plug in those values into my code I start to get compass bearings that make sense even when tilted. So, yes, the magnetometer appears to be working as expected.
Question is, is it normal to have a LSM9DS1 part out of the factory that never creates a positive magnetometer reading? No matter what position it is aligned in in the earth's magnetic field?
-thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.