2020-03-25 8:23 AM
HI Guys, I am looking for the MEMS Accelero meter for measuring the vibration in textile machines. Whether ST has the application example for condition monitoring system in machine or industrial automation.
If so please share the details
2020-03-25 8:34 AM
Hi @NGopa.1 , ST has available an evaluation tool kit, the STEVAL-BFA001V1B (LINK). for the predictive maintenance application in industrial environments, with several firmware examples. Alternatively I would suggest you one of the last ST kits, the STEVAL-STWINKT1 (LINK), to be interfaced with dedicated such as the IIS3DWB vibrometer adapter that can be directly applied on the textile machine to detect the vibrations (at this LINK). Regards
2020-03-25 9:04 AM
HI Eleon thanks for the reply. I will try the links
2020-03-25 9:05 AM
Actually i need the output of the sensor in mm/Sec instead of g. Is there any module available?
2020-03-26 1:43 AM
Hi @NGopa.1 , I don't think I've caught your request... mm/s is a velocity while g (mm/s^2) is an acceleration. To switch from acceleration to velocity you basically have to integrate the signal over the time (and it depends on the length of your acquisition). Regards
2020-03-26 4:02 AM
Yes exactly Eleon. My actual requirement is to acceleration into velocity. Is there any sensor available in ST that measures directly velocity mm/sec2. Or any calculation to convert the acceleration into Velocity (g to mm/Sec2)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.