MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

lsm6ds3 temperature compensation

Dear ST,As I tested with, the LSM6DS drifted follow temperature. As you can image bellow, red line is temperature and green is degree (was calculated from X, Y, Z )I'd like to confirm LSM6DS had internal temperature compensation? If NO, how to do it?...

0693W000000WIcWQAW.png
tpham.1 by Associate II
  • 4114 Views
  • 8 replies
  • 1 kudos

Heading values of sensor fusion library incorrect?!

I noticed wrong values for heading when using 9x fusion library. When placing board flat on the table, then tilt and move it and replace it to the exact same position as before, the heading value differs by up to 90 degree. There seems to be an issue...

marten by Associate II
  • 3018 Views
  • 4 replies
  • 0 kudos

6-point Calibration of Magnetometer

I am trying to calibrate a magnetometer using the 6-point tumble calibration described here: https://www.st.com/resource/en/design_tip/dm00253745-6point-tumble-sensor-calibration-stmicroelectronics.pdfI am getting confused when that method is applied...

CGrov.1 by Associate II
  • 2159 Views
  • 1 replies
  • 0 kudos

Resolved! LIS3MDL Temperature Compensation for Sensitivity

In the application notes it is stated that:"The sensitivity of the magnetic sensor changes when the temperature changes. A temperature compensation digital block is introduced to compensate for the effect of temperature."Does this temperature compens...

DRoyo.1 by Associate
  • 1728 Views
  • 2 replies
  • 0 kudos

steval-mksbox 1v1 BLE conenectivity range

I am using a steval-mksbox 1v1 and a rpi 3 to connect to it via ble usising the SDK. When I run one of the examples to connect, it detects the sensor during the scan, but when trys to connect "Unexpected error ocured". This happens when the distance ...

NMart.1 by Associate III
  • 1434 Views
  • 2 replies
  • 0 kudos

BlueNRG-MS framing error

I am having issues interfacing with the B-L475E-IOT01A's on-board SPBTLE-RF bluetooth chip. I am able to send header packets inquiring about the the bluetooth chip's write and read buffers. I have confirmed that I am doing this correctly, because I g...

WWale.2 by Associate II
  • 1021 Views
  • 1 replies
  • 0 kudos

Can someone provide a INTERRUPT BASED driver for LIS2DW12?

Hi community:There is this driver provided on ST webpage for LIS2DW12:https://www.st.com/content/st_com/en/products/embedded-software/mems-and-sensors-software/drivers-for-mems/c-driver-mems.htmlleading to:https://github.com/STMicroelectronics/STMems...

CPeng.1 by Associate
  • 1119 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.