cancel
Showing results for 
Search instead for 
Did you mean: 

IIS3DWB High-Rate FIFO/DMA Data Transfer on STEVAL-STWINBX1

Taha
Associate

Hi all,

I’m working on a project using the STEVAL-STWINBX1, and my main goal is to use the IIS3DWB vibration sensor as a high-speed vibrometer. I’m still pretty new to embedded programming (about 2 months in), so please bear with me!

Project setup so far:

  • Board: STEVAL-STWINBX1 (STM32U585AI MCU)

  • Using: Only the IIS3DWB vibration sensor (not the other sensors for now)

  • Peripherals: SPI2 (for IIS3DWB), UART2 (for debug/streaming), FreeRTOS

  • Goal: Read high-frequency vibration data, and eventually store it for later analysis

What I’ve tried:

  • I set up IIS3DWB via SPI2 and am running it at the full 26.7 kHz ODR (output data rate).

  • Because the data rate is so high, using an interrupt for every data-ready signal floods the CPU.

  • To handle this, I enabled the IIS3DWB internal FIFO (3KB, ~200 samples), set a watermark/threshold, and use the FIFO threshold interrupt to trigger reading.

  • My ISR releases a semaphore, which a FreeRTOS task then picks up to read out the FIFO using:

     
    iis3dwb_fifo_out_multi_raw_get(&dev_ctx, fifo_data, num);
  • After that, I try to send the samples out via UART (just for testing), and I have another task blinking an LED to check if the CPU is getting starved.

The problem:

  • If I try to send all the FIFO data out via UART (using HAL UART transmit, not DMA), the FIFO quickly overflows and I lose data.

  • It seems UART can’t keep up with the sensor, and the rest of the system starts missing interrupts/tasks.

  • (Side question: Does iis3dwb_fifo_out_multi_raw_get automatically clear the read data from FIFO, or do I need to manually manage FIFO pointers or clear it after reading?)

What I want to try next:

  • Move all heavy data movement (sensor-to-memory, memory-to-UART) to DMA, so the CPU can handle higher-level logic and avoid being starved.

  • My idea is:

    1. FIFO threshold interrupt fires → notifies a FreeRTOS task.

    2. The task reads data out of the FIFO into a buffer (possibly with DMA, if supported).

    3. Another task (or maybe same) sends the buffer out via UART using DMA as well.

  • I’m not 100% sure about the best way to architect this. My main goal is to reliably stream or store high-frequency sensor data without losing samples or overwhelming the CPU.

Questions:

  1. What’s the best practice for moving high-rate sensor data from the IIS3DWB FIFO to UART or storage on this hardware?

  2. Any gotchas with the DMA setup for SPI/IIS3DWB and UART on the STM32U5 series? Are there sample projects or HAL/LL code snippets for this?

  3. For those with experience: Do I need to “clear” the FIFO manually after reading, or does the read function automatically pop the entries? (Can’t find this clearly in the docs.)

  4. Any advice for task/interrupt/DMA priorities to make sure nothing is missed, especially as a beginner to FreeRTOS and STM32 DMA?

  5. If you have working code, a block diagram, or even just advice on the pipeline, I’d really appreciate it!

I’m just a student, so I’m still learning a lot of the STM32 and sensor stack. If you spot any flaws in my thinking or have a more robust architecture, please let me know! Open to all suggestions, links, or example code.

My repository is: https://github.com/YumTaha/STWINBX1/tree/FIFO-Tasks
I track my learning there so I can always have it if I want to implement functions together

another thing I ran into is all the examples and help out there is mostly for other sensors rather than IIS3DWB, I couldn't find anything about this sensor.

Thanks so much!

1 REPLY 1
Er1c
Associate

I too started my own drivers and had discovered inconsistencies that don't seem to reflect the datasheet.  Here's a ST driver for the IIS3DWB and some examples that were much more valuable to me than was the datasheet when it came to the firmware. STMems_Standard_C_drivers / iis3dwb_STdC at master · STMicroelectronics/STMems_Standard_C_drivers · GitHub

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.