MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ISM330DLC: Interrupt on Linux

Hello,I'm try using ISM330DLC connect to Linux OS on board IMX8MP via I2CLinux supported driver for this device (iio/imu/st_lsm6dsx); I added to dts file as below:&i2c5 { clock-frequency = <100000>; pinctrl-names = "default"; pinctrl-0 = <&pinctrl...

Tdo.1 by Associate II
  • 7722 Views
  • 6 replies
  • 0 kudos

Resolved! I am using the example project MEMSMIC1 in order to stream audio to host PC. But it is not working beside the following configuration: 2 channels, 16000 sample rate.

When I am changing the number of channels to 1 channel.it is recognized by the windows driver, but the"advanced" TAB is disappear (unlike 2 channels configuration). Did someone faced with this kind problem? Do I missedsomething? of course, audacity d...

AA.10 by Associate III
  • 2946 Views
  • 10 replies
  • 0 kudos

Sensortile box firmware

Which firmware version​ should be on sensortile box? Any other recommendations is much appreciated.​I am having issues with 2 of 2 sensortile boxes I received yesterday​. All interactions have been with Android st ble app. No response from one and...

MDupu.1 by Associate II
  • 3858 Views
  • 10 replies
  • 0 kudos

Synchronization of multiple ISM330DHCX

Hello,I need to use dual MEMS (ISM330DHCX) and MCU in my application for redundancy. Each MEMS is connected to a different MCU with independent supply. The data collected from sensors will be crossed checked if within a predefined tolerance. I think ...

JVinc.1 by Associate III
  • 6605 Views
  • 14 replies
  • 0 kudos

How to blink a LED with PNUCLEO

Please I really need help, I am using the P-Nucleo VL6180X, the purpose of my job is to command the opening of a door normally but before that I would already like to succeed in ordering the lighting of an LED.I use the stmicro API which I am trying ...

MSAMB.1 by Associate III
  • 1511 Views
  • 2 replies
  • 0 kudos

Faulty measurements from LIS2DW12

We have a small percentage of devices that once powered on show a certain issue.One or more axes of the accelerometer values are capped to the max or minimum value.This issue disappears when the device is powered off and powered back on.All the regis...

MDW by Associate II
  • 1835 Views
  • 3 replies
  • 0 kudos

Resolved! SWV Trace/Console for STWIN-STWINK1 on STM32CubeIDE, anyone was able to set up a trace on STWIN-STWINK1? Is this possible? Please let me know

HI All, I am using STWIN-STWINK1 for a predictive maintenance application, I am unable to set up SWV ITM data console and trace on STM32CubeIDE. I tried following all the tutorials on YouTube and community, nothing works. If anyone has been able to g...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.