Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Hi everyone!I have a LSM6DSO iNEMO inertial module (purchased in 2015) and I have some problems. I hope someone can help me. 1) Configuration of LSM6DSO. I have installed the Unico GUI program on my Windows PC, to configure my inertial module. When I...
The accelerometer is horizontal, in the Z axis 1g and I have about 500 mg in the X axis. I have 3 pieces of accelerometers and in similar positions I have different readings from the X axis.Temperature reads correctly.I found a certain inaccuracy:in ...
Hi, all.I am trying to figure out H3LIS200DL interrupt issue. Even if I have set interrupt threshold to high value, I can't see any pulse on INTx line. Also not sure what the INT1_THS register describes. Datasheet shows only 7 bit value.What I have d...
I tried to flash the FP-SNS-ALLMEMS1 firmware (https://www.st.com/content/st_com/en/products/embedded-software/mcu-mpu-embedded-software/stm32-embedded-software/stm32-ode-function-pack-sw/fp-sns-allmems1.html) to a brand new SensorTile over bluetooth...
I would like to be able to create a timer that counts time elapsed during an activity and resets when the activity stops. Any suggestions on how to do this.
Electronic designers can leverage worldwide “maker�? trend and use off-the-shelf easy-use platforms like Raspberry Pi for IoT demos or for evaluation purposes - at least as a starting point before you select a suitable component and eva board, tools,...
My application is uses a linear array (18 sensors) for object presence detection at a fixed distance (~70mm). A range threshold setting is used. The range measurement is not read, only the interrupt is used indicating the presence of a moving object....
I'm seeing the below issue with flashing firmware on the sensor tile device. I'm trying to test the ble_sampleapp for the sensor tile device. When I use the STM32Cube IDE with a nucleo board as a debugger, I'm able to run the code on the sensor tile ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.