MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Is there a IOC file for SensorTile example projects?

I am evaluating MEMS sensors using the SensorTile hardware and accompanying software (STSW-STLKT01). The toolkit has thus far been very nice. In order to move the project further I now want to port the AudioLoop example project to another MCU on a Nu...

Resistor changes for STEVAL-MKI196V1 and STEVAL-MKI109V2

Hi,On the MKI196V1 webpage (https://www.st.com/en/evaluation-tools/steval-mki196v1.html) It says that:"Changing the resistor settings is also compatible with the STEVAL-MKI109V2 motherboard"I cannot find any documentation on which resistor changes ar...

0693W000006EONBQA4.png
MSack.1 by Associate
  • 998 Views
  • 1 replies
  • 0 kudos

STEVAL-STLKT01V1: Firmware update.

Hello,I'm using STEVAL-STLKT01V1.Then, I downloaded ST BlueNRG GUI 4.0.0, which provides these firmwares into the Firmware\BlueNRG_stack directory:bluenrg_6_4b_Mode_2-16MHz-XO32K.imgbluenrg_6_4b_Mode_2-16MHz-XO32K_HCI.imgbluenrg_6_4b_Mode_2-32MHz-XO3...

Resolved! LSM303AH - Mag field on Z ax doubt

Hi, I have implemented a tilt and heading calculation using the simplified heading calculation that only works when the device is horizontal, and was until now ignoring the magnetic field value on the Z ax. Now I'm trying to implement a tilt compensa...

FGome by Associate II
  • 2790 Views
  • 4 replies
  • 0 kudos

implementing STSW-IMG009 API

first question about initiating const from adr 0x2D to 0x87, is not the internal addresspointer incrementing ?Second: The default device address is 0x29 or ?(datasheet says 0x52)

Ckjel.1 by Associate
  • 1107 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.