MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to get repeated threshold interrupt on LIS3DSH

Hi,I have setup the registers on the LIS3DSH according to the "Wake-up" example in application note AN3393. It works for the first interrupt, but so far i haven't had any luck to receive any more interrupts unless i read the OUTS1 register to reset i...

Klofs by Associate
  • 1287 Views
  • 1 replies
  • 0 kudos

DOUBLE TAP NOT WORKING IN LSM6DSO

Dear Concern, we are using LSM6DSO MODULE for my project purposeDouble Tap Issue :  Double tap is not working if we configured less than 208 Hz (Accelerometer ODR). Activity/Inactivity Interrupt Issue: At least one fake activi...

srao.1 by Associate II
  • 1316 Views
  • 1 replies
  • 0 kudos

Resolved! LIS2DE12 Vdd and VddIO power path

Hello,I'm developing an ultra-low-power circuit with LIS2DE12. I would like to have the accelerometer running with IRQ enabled, but serial communication shutted down.I can't understand at whitch power path the INT1 and INT2 are connected (Vdd or VddI...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.