2020-12-02 8:21 PM
I am currently working off of an Arduino to compute both Pitch and Roll, I do not need the Yaw axis. The application this is being done for requires arduino development so I dont have the opportunity to use a different platform.
I have both the Kalman Filter and Complimentary filter for testing and accurate estimation but I was wondering if there is any ST recommendation for Tilt Estimation on a 6-DoF IMU such as the ISM330DHCX.
The implementation will be within a Metal chamber so ideally no Magnetometer will be used,
I looked through the documentation and I am assuming there is no onboard computation for these factors, unless I am missing anything,
Any help is appreciated,
Thanks!
2020-12-03 12:22 AM
Hi @daethat ,
You may find some hints for your purpose (i.e. Pitch and Roll calculation with the gyroscope) in the Design tip DT0060, that exploits the gyroscope to update tilt measure and e-compass.
ST has developed STM32-related libraries for the angle calculations of ISM330DHCX device (and for the quaternion and device-orientation calculation), such as the MotionFX (doc1 and doc2), or the MotionDI dynamic inclinometer library.
>> I am assuming there is no onboard computation for these factors
There is no embedded integration in time of the gyroscope angular speed within ISM330DHCX fot the angles calculation, if I well understood your consideration. You have to perform it in "post-processing": this because, for an accurate angle calculation, it's important to run periodical real-time gyroscope calibration through angular zero-rate level coefficients (offset), aimed at correcting gyroscope data (e.g. the function implemented in the MotionGC).
-Eleon
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.