Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Hi, I am writing because after we changed our supplier we suddenly experienced a huge failure rate in our pressure sensors when our PCBA's arrived from our supplier. Both us and our supplier are a bit lost in figuring out the cause of this. until our...
I am using a LIS2DE12 however I can't get the current on the VDD_IO to drop below 25uA.Is there any reason for this?My current settings are:CTRL_REG1 = 0x3FCTRL_REG2 = 0x30CTRL_REG3 = 0x40INT1_CFG = 0x0AINT1_THS = 0x25I am running off a 3V supply.Che...
Specifically,https://community.st.com/s/question/0D50X00009XkXz9SAF/lis3dh-interrupt-int1-mode-not-firingI'm loged in but all that is shown is the question and a notice that the "This question is closed."Does that mean the question was never answered...
Hi,In the LPS33WTR pressure sensor,I want to program the LPS33WTR FIFO to a certain pressure and configure the interrupt as Threshold-based interrupt.No Where have I found the duration of the Interrupt logic change. I want to use it as a HW trigger o...
I have a really simple application setup. I'm currently feeding in one PDM microphone. I'm using the SAI interface (code is attached). First there appears to be a bug in the ST code. The SAI_PDMCR register have a field to set up to 4 microphones (see...
We are using X-Nucleo-IKS02A1 board to test the vibration sensor using vibration monitoring example code. The FFT data of vibration sensor is observed using Unicleo-GUI.It is observed that the FFT data is not represented in Unicleo-GUI when FFT size ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.