MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! The ID value read by ism330dhcx chip is always 0

Hi, stThe MCU platform I use is nrf52840. The sensor uses steval-mki207v1. The hardware connection method is mode 1. The SPI mode of MCU is mode0, the frequency is 8MHz, and the bit order is MSB first. On this premise, no matter how many times I read...

6June.1 by Associate II
  • 3039 Views
  • 5 replies
  • 0 kudos

Would you like to watch our latest on-demand webinar?

High Precision Inclinometer for Industrial Applications: Learn how to create innovative solutions with the latest MEMS-based high precision tilt sensor for industrial applicationsWatch the 1-hour, on-demand webinar to discover the newest addition to ...

0693W000007DX1uQAG.png

LPS22HH reporting inaccurate raw pressure values

I am currently interfacing the LPS22HH component and have been encountering some very strange pressure data.Currently I am interfacing this in I2C mode and reading the pressure sensor values from PRESS_OUT_XL (28h), PRESS_OUT_L (29h) and PRESS_OUT_H ...

DN_1 by Associate II
  • 2082 Views
  • 1 replies
  • 0 kudos

LSM9DS1 SDO not tri-stated

I need several LSM9DS1 sensors one the same SPI line. However, I noticed that when CS is high, SDO (aka MISO) is not tri-stated but pulled down to GND.I thought this was due to the default double-interface (SPI/I2C), so I have enabled the I2C_DISABLE...

DMona.1 by Associate
  • 1102 Views
  • 1 replies
  • 0 kudos

Resolved! Need help in selecting an accelerometer for my application.

I want to ensure that the user fits our portable battery powered radar onto the back of a vehicle in the correct orientation. I want to monitor this using an accelerometer, I am considering using the LIS2DH12 but I'm not sure if this is suitable and ...

TMahm.2 by Associate II
  • 1608 Views
  • 3 replies
  • 0 kudos

Resolved! Temperature offset in LSM6DSRX's Temperature sensor

I'm using the temperature sensor in LSM6DSRX.In page 12 (4.3 Temperature sensor characteristics) of the Datasheet (see the image), what is "Toff" (Temperature Offset)?The Table 4 gives a range of -15 to +15 C for Toff, what is this range for? The Tab...

0693W000007Cwx3QAC.png
AFars.1 by Associate
  • 1839 Views
  • 2 replies
  • 0 kudos

Resolved! Anomalous acceleration values from some LSM6DSLs: are they damaged?

I've used a number of times LSM6DSL IMU sensors and I never had any problem with them: they are in general very precise and straightforward to use. However, in a recernt pre-production run, some accelerometers provided strange values on one or two ax...

ADi S.2 by Associate
  • 1741 Views
  • 2 replies
  • 0 kudos

Using LIS3DH with VDD only and using VDD_IO for setup only.

Question is if I can use LIS3DH with VDD only (3.3v) , and VDD_IO (1.8v) supply only during configuration ? And in this case, what power use INT1 and INT2 pins ? If possible to run on VDD only with having them working (at least as OD ?).Datasheet is ...

GLuts.1 by Associate
  • 1249 Views
  • 2 replies
  • 0 kudos

Resolved! HOW TO DEBUG BOOTLOADER USING CUBEIDE

hi, I am trying to debug the bootloader which comes with sensortile.box to change it for my requirements. In doing so I want to inspect how it works using debug session. But unfortunately, when starting to debug the session the curser doesn't even re...

MImda.1 by Associate III
  • 1429 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.