MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to read multiple IKS01A03 memory register with DMA over i2c?

Hi,I am currently working on DMA combined with I2C bus. I want to read acceleration data from IKS01A3 with HAL function HAL_I2C_Mem_Read_DMA(). I want to read at 6 different memory registers. How can I use that function to get it work properly? Can I...

LZure.old by Associate II
  • 2059 Views
  • 6 replies
  • 0 kudos

Why acceleration data of LSM303D on the Z-axis doesn't work?

Hi,I have a LSM303D, compass, and acceleration sensor. I can communicate with the sensor, and I get the magnetometer data on all of the axes, unlike the accelerometer. Accelerometer Z-axis data comes "-32760" all the time. I work on stm32f103c8t6Here...

0693W000007BYC6QAO.jpg
AÖzba.1 by Associate II
  • 2272 Views
  • 4 replies
  • 0 kudos

WHO_AM_I register value read as 0xFF

Hello ST Community,I have some hardware samples with LIS2DH12 accelerometer. For all the samples except one, the value of WHO_AM_I register is read as 0x33 (which is expected). However, for one of the samples, it is read as 0xFF. What could be the po...

AB.4 by Associate II
  • 1903 Views
  • 5 replies
  • 0 kudos

Resolved! LIS2DE12 supply 1,8v / 3,3v

Hello,I have an issue with my LIS2DE12, when i'm starting up my board i'm doing the configuration of the device and then i need to put the boad from 1,8V to 3,3V to communicate with an other component. BUT when I come back to 1,8V the LIS2DE12 have t...

GLE B.1 by Associate II
  • 3254 Views
  • 6 replies
  • 0 kudos

Resolved! LIS3DH offset correction

Hi,We've been using LIS3DSH for a few years now and are now searching for alternative sensor because of availability problems.In LIS3DSH there are offset compensation registers OFF_X(Y,Z) for fixing the read axle values with correction values stored ...

Resolved! H3LIS100DL: prevent interrupting sample to be overwritten/overrun

The H3LIS100DL has no fifo, and the ODR can be set to 400Hz. This would make it update the axes data each 2.5ms. I have programmed it to interrupt a mcu when a threshold is reached. This wakes the micro controller from deep sleep. Unfortunately it ta...

PArve.1 by Associate II
  • 2200 Views
  • 3 replies
  • 0 kudos

VL53L1-SATEL circuits question

Dear a ST engineer,​I had purchased VL53L1-SATEL and evaluated the function with NUCLEO-F401RE and "VL53L1 Gui". I connected VL53L1-SATEL board to NUCLEO-F401RE board directly through some wires.However the GUI didn't recognize the connection of VL53...

TYomo by Associate II
  • 1667 Views
  • 2 replies
  • 0 kudos

Resolved! LIS2MDL Axis Directions

Figure 2 of the LIS2MDL datasheet shows the following picture of the magnetometer axes orientation. However, it's completely unclear if they are labeling the positive direction of the axes. If they did label the positive directions with the X/Y/Z lab...

JCond by Associate
  • 2153 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.