MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM6DSL Gyro 800Hz Noise

Hello,When configuring the LSM6DSL ( STEVAL-MKI178V1 ) to sample Data at 6664 HZ ( without any digital Filters active, FS= +- 16g, +- 250deg/s ) there seems to be an consistent 1deg/s @ 800Hz noise on some gyro axis. The same signal but stronger ( > ...

0693W000007CTzeQAG.png 0693W000007CU0DQAW.png
JWoeb.1 by Associate II
  • 2088 Views
  • 3 replies
  • 0 kudos

Resolved! About FIFO of gyro sensor I3G4250D

Is it stored in the FIFO when the threshold of the INT1_THS register is exceeded?Or is it stored regardless of the threshold of the INT1_THS register?

HIMAM.1 by Associate
  • 1570 Views
  • 2 replies
  • 0 kudos

LSM9DS1 Gyro drifting while shutdown

I have an application with a LSM9DS1 that is powered up for a few minutes at a time and then shutoff. It might be powered up again for a few minutes within the same day, or be used only the day after or a few days later. The purpose is to get angular...

PRebo.1 by Associate II
  • 1781 Views
  • 2 replies
  • 0 kudos

Resolved! LIS2DE12 generating interrupts at low ODR

I am trying to get the LIS2DE12 to generate an interrupt when shaken. I have connected the INT1 pin to an open drain I/O pin of my MCU. I an get it to generate the desired interrupt with some reliability. However, when it is just sitting still, it ge...

RKeit.1 by Associate III
  • 1713 Views
  • 2 replies
  • 0 kudos

Resolved! LIS2DE12 self test

I am trying to set up a self test process for an assembly including an LIS2DE12. The device works normally when I tilt and invert it. When I try to put it in to self-test mode by writing either 02h or 04h to CTRL_REG4 the readings are the same as wi...

RKeit.1 by Associate III
  • 3646 Views
  • 6 replies
  • 0 kudos

Resolved! Getting invalid readings in steady-state.

Hello Community,I am working on the LIS2DE12 accelerometer. using the example code by STM.https://github.com/STMicroelectronics/STMems_Standard_C_driversI am making a test case with the lis2de12_filter_hp_rst_on_int.c example.I have placed a module o...

spati.11 by Associate II
  • 4619 Views
  • 9 replies
  • 0 kudos

VL53LX Range sensor API size optimization

Hi everyone,I try to implement range measurement using the VL53L3CX sensor with the VL53L3CX_API_1.1.4. I can get distance measurement and talk with the sensor properly using the basic patent :Status = VL53LX_WaitDeviceBooted(Dev); Status = VL53LX_Da...

Ben1 by Associate III
  • 2026 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.