MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L1X does not boot.

I recently purchased VL53L1X ToF laser ranging sensor and for the last couple of weeks I am trying to make it work. Based on reference schematic from the datasheet I built the following setup:Using STM32L011 uCU, ULD API and LowLevel I2C libraries ...

0690X00000ArVMTQA3.jpg 0690X00000ArVPrQAN.png 0690X00000ArVQ6QAN.png 0690X00000ArVQLQA3.png
velizarw by Associate II
  • 8138 Views
  • 13 replies
  • 0 kudos

Hello, I am trying to interface MP34DT001 MEMs microphone on STM32 BL475E Discovery iot board. I have tried using BSP for interfacing microphone but I am getting error in initializing BSP_AUDIO_IN_Init(AUDIO_INSTANCE, &MicParams) it is returning -9

I have checked -9 means failed to set clock. I have run debug trace on it, I have attached the point where it is thowing error. I am new to this kindly someone guide me what I am doing wrong. Or kindly point me toward any working implementation of MP...

0693W000005BGDSQA4.jpg 0693W000005BGDDQA4.jpg
WIsa.1 by Associate
  • 1813 Views
  • 2 replies
  • 1 kudos

VL53L1_PRESETMODE_RANGING, VL53L1_GetMeasurementDataReady()

Calling   status = sensor_vl53l1.VL53L1_GetMeasurementDataReady(&NewDataReady);from the Example, I get only status = 0 and NewDataReady = 0;I stepped into the functions down to the Device access via I2C.All went well so far. I got: gpio__tio_hv_...

ritzeng by Associate II
  • 1209 Views
  • 1 replies
  • 0 kudos

VL53L1 2.0 Library

Unused code detected:VL53L1_Error VL53L1::VL53L1_RdByte(VL53L1_DEV Dev, uint16_t index, uint8_t *data){ int status; status = VL53L1_I2CRead(Dev->I2cDevAddr, index, data, 1); //FR bug :: I2CRead exits always with 0! why the following check? Unused...

ritzeng by Associate II
  • 2207 Views
  • 3 replies
  • 0 kudos

Resolved! How to use X-CUBE-CELLULAR Framework with the STEVAL-STWINKT1 and Quectel BG96 on STMOD+ connector? Framework confusion.

What I have:SMT32 CubeIDE 1.3.0the P-L496G-CELL02 eval kit with the Quectel BG96 on STMOD+ connectorthe X-cube-cellular examples for connecting the board with the cloud via MQTTan STEVAL-STWINKT1, which I want to connect via MQTT to our cloudserviceW...

PLang.3 by Associate II
  • 8593 Views
  • 17 replies
  • 1 kudos

Resolved! Guaranteed specs on the ISM330DHCX specially accelerometer part

Hello support team,We are decided to use your ISM330DHCX for our next products. So we are ongoing to describing the FW requirement to the FW team in our organization.However, I’m not sure we should use the USER OFFSET registers in device for the offs...

IMaru.1 by Associate
  • 1996 Views
  • 2 replies
  • 0 kudos

Resolved! AlgoBuilder: Load design failed

Hello,When I try to open a saved design I receive message "Load Design Failed!".It was previously updated with AlgoBuilder v 2.8.0.4490.Please find xml fileThank you for your help!Best regards,Jean

jpo92 by Associate II
  • 2023 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.