2020-07-09 4:57 AM
What I have:
What I already did:
What is my goal?
Problem:
Questions:
What would be the more future proof path? Adapting the AWS-cloud example or using X-CUBE-CELLULAR as base framework?
Thanks for your help and best regards
Patrick
Solved! Go to Solution.
2021-03-30 3:11 AM
Hi @Chandrashekar C ,
Our experts performed some tests (described here below) without encountering issues. The outcome is that your issue could be related to supply problems.
Test configuration:
HW
FW
Please find attached the log files.
The modem obtains the IP address and can configure RTC from both www.gandi.net and www.st.com.
Their suggestion is:
-Eleon
2020-07-17 3:21 AM
Hi ST-Support, can you please help me? The topic is still open. Best regards, Patrick
2020-07-23 4:43 AM
I'm interested on the answer also.
Thanks
2020-09-15 4:42 AM
Hi @PLang.3 ,
sorry to come to you so late. Looks like a quite a complex topic, but me please check internally by our experts.
I'll keep you updated.
-Eleon
2020-09-21 4:30 AM
Hi @PLang.3 , @a123 ,
back to you with some updates.
The STSW-STWINCELL software package is based on the STM32CubeExpansion_Cloud_AWS_V1.4.0, which uses the Cellular Framework V3.0.0.
The current Cellular Framework version is the V5.1.0, and it is the only version available for the download on st.com.
The two versions are quite different: for this reason, our experts say that an alignment of the STSW-STWINCELL with the Cellular Framework V5.1.0 would be very difficult.
-Eleon
2020-09-21 7:05 AM
Hi Eleon,
first of all, Thank you very much for this information. So am I right in assuming that the X-CUBE-CELLULAR framework will be further developed? Current version is the V5.1.0.
I would like to use the STEVAL-STWINKT1 as evaluation hardware together with the Quectel BG96 on STMOD+ connector.
So for my project it would be best to use the X-CUBE-CELLULAR-Framework V5.1.0 and adapt it so that it works with STWINKT1, right? Or is there already a suitable example software available here??? After all, STWINKT1 is a current ST evaluation board that is also designed for connectivity and the X-CUBE-CELLULAR framework is the ST software for this. So why dont you go this way?
Best regards, Patrick
2020-09-22 12:24 AM
Hi Patrick,
you are right, the eval tool and the last X-CUBE-CELLULAR-Framework should be aligned together. I'll report this point internally, but our engineers should already be aware of this. I would suggest you to use the STWINKT1 + Cellular framework version 3.0.0 and start from this project trying to adapt it to version 5.1.0 framework. You can find the past X-CUBE-CELLULAR packages HERE.
-Eleon
2021-03-01 5:52 AM
Hi @Eleon BORLINI ,
Any idea when the new version of STSW-STWINCELL shall be released? it seems to be one year old now.
really appreciate if you share any information on new version of STSW-STWINCELL.
Kind Regards
Chandrashekar C
2021-03-01 6:09 AM
Hi @Chandrashekar C ,
unfortunately no news so far on this specific topic, but in the meantime we upgraded the hardware from the STWINKT1 to the STWINKT1B, so I'm expecting the function pack version update will follow accordingly, assuring -hopefully- a back compatibility between the two platforms.
-Eleon
2021-03-01 6:17 AM
Hi @Eleon BORLINI ,
Thanks for the quick response. Currently we are using STWINKT1B with STMod+ for our development. Looking forward for the updated function pack. I hope they release it soon.
Kind Regards
Chandrashekar C
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.