MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! BMI055 interrupts problems

Hello,I am writing a code to initialize the BMI055 IMU on my STM32F765. To do so I am using the HAL libraries to enable the SPI connection through DMA and the drivers provided by Bosch: bma2x2 and bmg160.The two sensors work perfectly when only one o...

FUs.1 by Associate III
  • 7639 Views
  • 13 replies
  • 0 kudos

Resolved! Examples Operation codes for commands for LS3DSH

Hi,I can't find any examples of using commands in the statemachines.I want to create a tilt sensor, by using 2 statemachines, 1 is monitoring x axis, the other z axis.To keep it simple i will add the code for the x axis only . This statemachine setup...

sde c.1 by Senior II
  • 3364 Views
  • 9 replies
  • 0 kudos

No output issue from MP23ABS1 on the old version of STWINKT1.

I have two different HW versions of STWIN and there is an analog mic difference; MP23ABS1 vs MP34ABSU. When I test with MP23ABS1, it looks it has some issue that it doesn't output sound data at all. but, the new revision with MP34ABSU hasn't that iss...

TKIM.3 by Associate
  • 3310 Views
  • 7 replies
  • 0 kudos

P-NUCLEO-IKA02A1 EVK

Hi Sir/Mdm,I tested the EVK with the lowest PPM in clean air was 6ppm yesterday and today I tested again in clean air was 2.4ppm and is fluctuating. When I first got this EVK, it was 0.6ppm which < 1, after testing a few rounds with CO gas, then I wo...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.