MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Requirement power supply to LIS2DH12

Dear all,I'm researching and designing hardware on this mems LIS2DH12. But I can't find any parameters ralative to noisy, ripple voltage ... to make sure perfomance of accel.So could you share some documents about hardware design note?? I'm going to ...

TNguy.15 by Associate
  • 970 Views
  • 1 replies
  • 0 kudos

On the LPS22HB SPI, what is the minimum high time for CS?

I'm communicating via SPI with an LPS22HB using an FPGA. Is there a minimum time specification between SPI transactions? I'm currently setting CS high for 0.5 SPC cycles between transactions, but this doesn't seem to work.

JPhil.3 by Associate
  • 1157 Views
  • 1 replies
  • 0 kudos

VL6180 always sending VCSEL Watchdog error

Hello,I was designing a board with a VL6180 and was surprised that the 0x4F register never uptaded to tell me that a new measurement was finished.So I looked at the 0x4D register to see that it answered me 0x19. Whitch mean I have a VCSEL continuity ...

SSchm.5 by Associate III
  • 1517 Views
  • 2 replies
  • 0 kudos

Resolved! VL53L1CX (DocID031281 Rev 3) question about IOVDD & 2V8 mode XSHUT - needs pull up resistor or can it be direct connected to AVDD?

Question #1:In my system, I have 3.3V available, so I was planning to use that for AVDDVCSEL & AVDD since it is within the range but the I2C interface will run at 1.8V.The 1.8V seems fine from a Vih/Vil point of view. My concern is around IOVDD and 2...

FusionFX and quaternions - stationary drift

Hello, I'm using the FusionFX library(V2.5) to calculate quaternions and therefore estimate an object position. I'm using an X-NUCLEO-IKS01A3 that has the  LSM6DSO (ACC + Gyro) and LIS2MDL ( Mag). I'm using an 16G scale in acc and 2000dps in the gro...

PLuze.1 by Associate II
  • 2222 Views
  • 3 replies
  • 0 kudos

Resolved! LIS2DTW12 I²C/SPI mode selection

I want to read LIS2DTW12 data using SPI which is also shared with another device, can I use the LIS2DTW12 CS pin as chip select and operate devices one by one.because according to the LIS2DTW12 datasheet:State of CS1: SPI idle mode / I²C communicatio...

Aishwarya by Associate III
  • 1710 Views
  • 2 replies
  • 0 kudos

Resolved! LIS2HH12 and IIS2DLPC two's complement temp compared

Hi all,I'm currently deploying hardware that can have either the LIS2HH12 or IIS2DLPCAccording to the datasheet the LIS2HH12 stores the temperature as two's complement / 11 bit / 8 digit per degrees celcius.So I convert it this way:int16_t tilt_read_...

WSpar.1 by Associate III
  • 7593 Views
  • 19 replies
  • 0 kudos

Resolved! LSM303AGR SPI operation

Posted on March 01, 2018 at 11:24Hi,I am struggling with moving from the obsolete LSM303D sensor to the LSM303AGR sensor.I had the LSM303D sensor working correctly in continuous mode with the STM32F1 processor using 4 wire SPI mode.But I cannot get ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.