2021-04-15 6:06 PM
Hi Sir/Mdm,
I tested the EVK with the lowest PPM in clean air was 6ppm yesterday and today I tested again in clean air was 2.4ppm and is fluctuating. When I first got this EVK, it was 0.6ppm which < 1, after testing a few rounds with CO gas, then I won't drop to that point. Appreciate if you could give us some support on this problem, thanks.
2021-04-16 12:30 AM
Hi @jason239955_st ,
I'm not an expert of gas sensor, since it is not from ST but from this other company, Figaro (TGS5141-P00).
I see from the datasheet (that you can also find in attachment to this post) that there could be up to ±10ppm equivalent offset, but I don't know whether it can fluctuate...
As a standard procedure we suggest for our environmental sensors, I would suggest you to run a 85°C bake, to clean any post-solder effect.
My first suggestion is however to directly contact Figaro for an effective help.
Let me then know if you can find out more from their side.
-Eleon
2021-04-16 2:02 AM
Hi Eleon,
I am using this evaluation board with the Nucleo-L053R8 to do the evaluation and getting the result of the CO sensor.
After testing a few rounds, I noticed there was a setting "T" on the for test the sensor using the NUCLEO together with the sensor expansion board.
I keep getting error while try to run the test procedure, screenshot attached
Datasheet not mention the test procedure, I am confused with the error message "JP2 pin 1 was not connected" what does that mean? and what should I do?
JP2 on the sensor expansion board is GAIN settings, I tried shorted pin 1-2, same error, and tried shorted 2-3 also same error. Appreciate if you could help on this issue.
2021-04-20 4:01 AM
Hi @jason239955_st ,
Are you using the board with the default firmware uploaded?
As another interface channel, as shown in the UM2247 user manual, p.11, you could use also Unicleo-GUI to interface the board. It contains a Custom Fields window which fully supports the P-NUCLEO-IKA02A1 expansion board to show the measured values in a graph. The source code for NUCLEO-L053R8, NUCLEO-F401RE and NUCLEO-L476RG boards is available in the X-CUBE-IKA02A1 software package as DataLogCustomLite sample.
Did you already tried this solution?
-Eleon
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.