MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Data sampling of ISM330DLC

Hi! I am using ISM330DLC to get data from all three gyros and three accelerometers with an ODR of higher than 400Hz. When the circumstance temperature is going down from normal to about -20~-30℃, there are several disturbance in outputs of gyros (dif...

BLee.3 by Associate II
  • 2736 Views
  • 4 replies
  • 0 kudos

Option "Enable Admin Panel" in DSH-PREDMNT1 serverless.yml file. Can someone explain this option and what is the purpose of this Admin Panel in DSH-PREDMNT1.

In DSH-PREDMNT serverless.yml file there is an option as below... # uncomment to deploy admin panel # - Outputs: #   AdminIdentityPoolId: #    Value: #     Fn::ImportValue: AdminIdentityPoolId #   AdminPoolId: #    Value: #     Fn::ImportValue: Admin...

Vchak.11 by Associate II
  • 3073 Views
  • 1 replies
  • 0 kudos

lsm6dsox interrupt

Hi,I want to read sensor data periodically in interrupt mode.And sensor is configured like below code. /* Set Output Data Rate */ lsm6dsox_xl_data_rate_set(&lsm_ctx, LSM6DSOX_GY_ODR_3333Hz); lsm6dsox_gy_data_rate_set(&lsm_ctx, LSM6DSOX_GY_ODR...

0693W00000APnfXQAT.png 0693W00000APnfSQAT.png
JPARK.2 by Associate II
  • 1441 Views
  • 1 replies
  • 0 kudos

SensorTile Box- Steval Mksbox1V1

Hi, Am trying to generate the C-code for the ASC (Acoustic Scene Classification) model from the FP-AI-SENSING1 Pack through Stm32cube mx. But I can see there is changes in the code between existing code and the new code which was generated by me. I ...

Resolved! LIS2DW12

There saw that there is no gyroscope in this model, so I dont understand how we can to differentiate between (for example) - stationary mode, when we have g in the X axis and '0' on the other. AND movement so there is g in X axis and '0' on other axi...

Msaga.1 by Associate II
  • 3754 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.