MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to initialise a LSM6DSRX sensor ?

Hello, I am trying to implement a simple program on my STM32 NUCLEO F302R8, that reads data from a LSM6DSRX iNemo module (STEVAL MKI195V1) throught a NUCLEO-IKS01A2 extension board, and stores it in flash memory.I am unable to find any kind of docume...

LARBE.1 by Associate II
  • 1690 Views
  • 2 replies
  • 0 kudos

PDM2PCM example code

Hello,I am trying to understand the PDM2PCM conversion using I2S as the receiving protocol. Does anyone have an easy example for generating a single PCM sample from the PDM data bits? I am having some difficulty doing this using the VM3000 PDM MEMS...

kcire L. by Associate III
  • 5586 Views
  • 5 replies
  • 0 kudos

LIS2DH12 acc calibration how to enable

Hi Everyone, excuse meI have developed android 9 system using imx6 motherboard.after finished HAL integrated due to calibration needed.how can I enable LIS2DH12 acc calibration functionI can see the STMems_Android_Sensor_HAL_Input-STMems_Android_Sens...

Victor3 by Associate
  • 1598 Views
  • 2 replies
  • 0 kudos

Heart rate sensor output

Hi I’m using an arduino heart rate sensor on the nuclei f411re board and I am getting output values of 2000-3500 when not pressed and values between 0-10 when pressed I can’t find much information about it online and I was wondering what do these num...

MMori.6 by Associate
  • 1131 Views
  • 1 replies
  • 0 kudos

LSM6DSOX Tap and Double Tap configuration

I would like to pick up both single and double taps in my application. I have the double tap working but cannot get it to pick up a single tap. In reading the TAP_SRC register , the TAP_IA bit shows a 1 for a double tap but never does for a single...

RAtki.3 by Associate II
  • 3025 Views
  • 5 replies
  • 0 kudos

LSM303AGR Accelerometer can't generate interrupt at INT2 pin

Hi sir,I have a custom board containing LSM303AGR connected to stm32f407vg via I2C.I can generate interrupt at INT1 pin.What is the correct initialization to enable LSM303AGR Accelerometer activity/inactivity function Interrupt 2?Our initial setting:...

Whung.1 by Associate
  • 1866 Views
  • 3 replies
  • 0 kudos

Resolved! problem with Lis2dw12 data ready interrupt.

Hi!I'm using lis2dw12 on a custom board and trying to acquire the acceleration based on the data ready signal that I routed to INT1.The code was based on this repository but I think I'm doing something wrong because I can't get any signal from the...

MRive.2 by Associate
  • 2471 Views
  • 3 replies
  • 1 kudos

Resolved! I am using IIS2DH accelerometer sensor with stm32wb55 for Vibration Sensor application. I am having tech query listed below, 1) Range of X ,Y and Z axis raw data. 2) Range of X, Y and Z axis in mg 3)How to calibrate X , Y and Z (Raw data / mg ?)

4) Which FFT algorithm is best for my application (RFFT/CFFT)5) After FFT will i get three output for x , y , z or only 1.6) Output example of after FFT.

HPate.7 by Associate II
  • 3455 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.