2021-06-09 6:31 AM
Hello
Sampling data from the IIS3DWB accelerometer over the course of a couple of seconds, when the device is completely stationary, on the 16g range, the peak-to-peak readings on each axis are:
p2p x = 0.0566g
p2p y = 0.0634g
p2p z = 0.1215g
These seem to be quite excessive detected movements; and assumed it was the noise floor (!!!) of the device. A bit of digging on these forums suggested enabling the LPF2; which I did, at ODR/100. The results improved, to:
p2p x = 0.0151g
p2p y = 0.0122g
p2p z = 0.0166g
But these too still appear quite large given the completely static nature of the device.
Are these results to be expected? Is this the noise floor of the MEMS device, ADC, other internal circuitry?
Kind regards
Gary Partis
Solved! Go to Solution.
2021-06-23 2:10 AM
HI Eleon
Many thanks for your reply.
Instead of using our product, we purchased a STEVAL-MKI109V3 "motherboard" for trying out the accelerometer with quick changes to settings; and found that enabling the high pass filter, with a low cut-off frequency (ODR/800); then the noise was roughly equal above and below the zero point, allowing for an average of almost zero.
This allows our Vrms calculations to work nicely on our product, although we are now virtually "deaf" to very low frequencies.
We are making all filter settings configurable from a user front end to add flexibility.
Kind regards
Gary
2021-06-14 3:28 AM
Hi Gary @GPart.1 ,
consider please the datasheet, p. 5.
The declared Linear acceleration zero-g level offset accuracy is typically ±60mg, with maximum range [-180mg, +180mg].
So, considering these specifications, the values you are measuring on the 3 axis are in spec.
You can improve the values in a couple of ways:
If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster.
-Eleon
2021-06-14 4:53 AM
Hi Eleon.
Many thanks for your answer.
We also perform offsetting of all 3 axes, but after data has been read from the device; to allow for varying installation orientations.
Essentially, is there any magic that I may perform to remove the random "jitter"? Is this from ADC noise etc?
Kind regards
Gary Partis
2021-06-23 1:03 AM
Hi Gary @GPart.1 ,
if you have no current consumption constrains and your target is only to improve the "resolution"/repeatability performances, you can try by averaging the output data in your code: in this way you'll smooth the signal variations and decrease the noise too.
Regarding the noise floor, you can check the datasheet p.5: it is down to 75 µg/√Hz in 3-axis mode / 60 µg/√Hz in single-axis mode
-Eleon
2021-06-23 2:10 AM
HI Eleon
Many thanks for your reply.
Instead of using our product, we purchased a STEVAL-MKI109V3 "motherboard" for trying out the accelerometer with quick changes to settings; and found that enabling the high pass filter, with a low cut-off frequency (ODR/800); then the noise was roughly equal above and below the zero point, allowing for an average of almost zero.
This allows our Vrms calculations to work nicely on our product, although we are now virtually "deaf" to very low frequencies.
We are making all filter settings configurable from a user front end to add flexibility.
Kind regards
Gary
2021-06-23 2:12 AM
Thanks Gary for the feedback!
That's good
-Eleon
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.