MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS2DW12TR acceleration values not returned

I am using the Accel 10 click housing the LIS2DW12TR accelerometer and I want ot run it using a MicroPython program.The code is as follows:https://github.com/Yadnik1/Accel-10-i2c/blob/main/Accel10i2c.py .It does not detect the sensor and I am skeptic...

YBend.1 by Associate III
  • 1095 Views
  • 1 replies
  • 0 kudos

Resolved! IIS3DWB FIFO counter does not decrease when reading.

Hi,I'm testing IIS3DWB MEMS accelerometer. It is set FIFO in continuous mode and FIFO watermark WTM[7:0] = 256.FIFO threshold interrupt on INT1 pin is enabled.The uC reads 256 data (7 bytes each) from FIFO_DATA_OUT_TAG as soon as INT goes high. Data ...

Palmering by Associate II
  • 2087 Views
  • 2 replies
  • 0 kudos

LPS22 pressure not accurate or damaged?

Hello,I have made a custom board with lps22hb. I am trying to get accurate pressure but it fluctuates with time. As I plotted a graph showing pressure and temperature I figure there is a direct relationship. I think that according to the datasheet, i...

0693W00000D2Du8QAF.png
BDELR.1 by Associate II
  • 2294 Views
  • 4 replies
  • 0 kudos

Resolved! Data rate vs Data reading rate in mems sensors

Hi,I am configuring the mems sensor data rate as 30hz,So what should be the data reading rate in this case. I mean is it necessary to put a delay after configuring the sensor for reading data continously Or we have to check the status of data ready...

Interfacing with onboard i3g4250d gyroscope on STM32F429i

I have been trying to test and get the gyroscope to communicate via SPI for a bit however it just seems to *refuse* to respond. As per the User manual for the board UM1670, PC1 is CS, PF7 is the serial clock, PF8 is MISO, and PF9 is MOSI all for SPI5...

SAgaz.1 by Associate II
  • 3780 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.