MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VL6180V1 for measuring the level of water - Will it give me the height of water or distance of water from sensor

Hello. I would like to measure the level of water in a closed container.I have chosen VL6180V1 for the same since it has an 850 nm light source which won't be absorbed by water.I have referred this article for it:https://community.st.com/s/question/0...

Resolved! LIS3DH Address Changes Post-Config

I am using a LIS3DH breakout board that is exhibiting weird behavior. My I2C master is a STM32L496 board that has been tested OK with other I2C chips.StartupI2C init to 400 KHzScan all possible addresses via HAL_I2C_IsDeviceReady() loop Remember add...

jrgert by Associate III
  • 2040 Views
  • 2 replies
  • 0 kudos

STEVAL-MKI159V3 , I2C DATA not renewal.

It seems to read the data normally at first.After that, it keeps getting the same data.Moving the sensor does not change the data value.Is there any other command I need to pass before getting the value?I know you are busy, but please reply.upload im...

YKang.3 by Associate II
  • 2036 Views
  • 4 replies
  • 0 kudos

LIS2HH12 Works for a moment and then stops working, value of 0 is being returned.(Using Arduino on a custom atmel328p board)

We have been using the LIS2HH12 accelerometer and it will work on a fresh board for about a day or so and then stop working. Below is some stripped down code from this library:https://gitlab.com/rhombio/rhio-libraries/rhio-LIS2HH12/-/blob/master/exam...

0693W00000D2NHfQAN.png 0693W00000D2NHuQAN.png
CPhip.1 by Associate II
  • 1271 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.