MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! H3LIS331DL: Self-test function available?

I am wondering wether this device offers a self-test feature similar to its low-g cousin, the LIS331. I noticed that there is an app note attached on the product page of the H3LIS331DL that specifically describes the self-test feature in ST’s MEMS se...

YIbra.1 by Associate II
  • 2726 Views
  • 4 replies
  • 0 kudos

Resolved! Steval-STWINKT1B - Where is all the power going?

On the STEVAL-STWINKT1B board, and using the HSDatalog firmware, it uses about 60mA in idle state. I have disconnected the sensors, and the uC, and turned off the SD card power lines, but it's still at around 2mA. Does anyone know where this power ...

LWeir.775 by Associate II
  • 3132 Views
  • 6 replies
  • 0 kudos

Resolved! How to configure AcousticBF library for PCM mode?

Are here any example projects on how AcousticBF library should be configured exactly for PCM mode? There are plenty of examples for PDM mode configuration, but none for PCM, which is frustrating, since the documentation on this library is not very ex...

PIvan.9 by Associate II
  • 2280 Views
  • 2 replies
  • 0 kudos

LSM9DS1 WHO_AM_I REGISTER (0x0F)

Hello, I have difficulties to get value of 0x68(IMU) and 0x3D(Magnetometer) from LSM9DS1 WHO_AM_I Reg 0x0F. I did on custom made board with STM32L083RZ and use I2C communication to LSM9DS1. I am using I2C3 PortC pin 0 and pin 1. The SDA&SCL are both ...

ABin .1 by Associate II
  • 2382 Views
  • 2 replies
  • 0 kudos

Resolved! VL53L1x People Count by using Interrupt method

Dear Team,We are using VL53l1X in our application to detect people leaving and entry, we got 5 vl53l1x breakout boards from one of my distributors for prototyping.People count programming working without any issues when using it in polling/continuous...

MMari.2 by Associate
  • 1671 Views
  • 1 replies
  • 0 kudos

LSM6DSO pedometer interrupt setting

Hello,I am using LSM6DSO sensor to do a pedometer. I use the official interrupt signal to control the step update like the following sentence.int1_route.emb_func_int1.int1_step_detector = PROPERTY_ENABLE;But I found the interrupt signal always has so...

JXiao.1 by Associate II
  • 1728 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.