2021-09-02 7:36 AM
Hello,
I am using LSM6DSO sensor to do a pedometer. I use the official interrupt signal to control the step update like the following sentence.
int1_route.emb_func_int1.int1_step_detector = PROPERTY_ENABLE;
But I found the interrupt signal always has some delays. When I am moving, sensor will not produce an interrupt signal. After I stop moving for few seconds (about 10 seconds), the sensor will send an interrupt signal.
Is there some settings for this condition?
Thank you.
2021-09-07 7:42 AM
Hi @JXiao.1 ,
Are you using the lsm6dso_pedometer.c Github reference code?
And did you set the proper ODR and FS, as stated in the application note AN5192, p.58, of // ODR_XL = 26 Hz, FS_XL = ±4 g?
I suggest you also to enable the False-Positive Rejection and Advanced Detection blocks, as suggested in the code below:
/* Enable step counter */
lsm6dso_****_sens_set(&ag_ctx, LSM6DSO_FALSE_STEP_REJ_ADV_MODE);
emb_sens.step = PROPERTY_ENABLE;
emb_sens.step_adv = PROPERTY_ENABLE;
lsm6dso_embedded_sens_set(&ag_ctx, &emb_sens);-Eleon
2021-09-07 8:20 AM
Hi Eleon,
I have seen the reference code. But the reference code use while loop instead of interrupt. The while loop will take more power consumption.
The ODR_Xl is set 26 Hz and FS_XL is ±2g. This is the code for pedometer.
lsm6dso_xl_full_scale_set(&imu_dev_ctx, LSM6DSO_2g);
lsm6dso_gy_full_scale_set(&imu_dev_ctx, LSM6DSO_250dps);
lsm6dso_block_data_update_set(&imu_dev_ctx, PROPERTY_ENABLE);
lsm6dso_****_sens_set(&imu_dev_ctx, LSM6DSO_****_BASE_MODE);
lsm6dso_pin_int1_route_get(&imu_dev_ctx, &int1_route);
int1_route.emb_func_int1.int1_step_detector = PROPERTY_ENABLE;
lsm6dso_pin_int1_route_set(&imu_dev_ctx, &int1_route);I will try your pedometer working mode. Thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.