MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! DTS configuration for LIS2DW12

Hi,I am trying to figure out how to determine the reg=<0x??> value for the LIS2DW12. From the example page they have 0x6b but for a different device. I cannot figure out what this value needs to be.Thanks&i2c2 {       status = "ok";       #address-ce...

BCour.1 by Associate
  • 1469 Views
  • 2 replies
  • 0 kudos

LIS2DW12 not recongnizing movement

Hello , I am working with accelerometer LIS2DW12, when I move the device very very slowly I do not see that an INT1 interrupt being raised. However, when I move the device in regular speed I DO see the interrupts. Can you tell me why is that?(the mov...

Msaga.1 by Associate II
  • 1159 Views
  • 1 replies
  • 0 kudos

Resolved! Configuring the Meta classifier whith UNICO

Hello,I'm working on an ultra low power application where the MLC of the LSM6DSO32X is used to wake up the mcu when interesting stuff is happening, in particular I implemented two decision trees, each one focused on the detection of a pattern.In orde...

0693W00000FAB3GQAX.png
DGiov.1 by Associate III
  • 1523 Views
  • 2 replies
  • 0 kudos

STEVAL-MKI159V1 with Nucleo F446RE - I2C

Hi, it's my first experience with MCUs in general.In this first approach I try to read outputs from MKI159V1 (LSM9DS1) with the nucleo F446RE. I'm starting with I2C protocol. I read any kind of articles here in the community but I still can't work it...

Occio by Associate
  • 1288 Views
  • 1 replies
  • 0 kudos

H3LIS331DL: Getting terrible readings

I'm experimenting with this accelerometer and I'm having some very disputable results while the device is sitting still.I'm using ST's library code, but I will detail what I am doing here:h3lis331dl_full_scale_set(&dev_ctx, H3LIS331DL_100g); h3lis331...

Corrupted Data on the SD card from STWINK HS Data Logger

Reducing the number of sensors enabled in the configuration file helps, as does slowing down the SD clock (i.e. increasing hsd1.Init.ClockDiv = n in STWIN_sd.c). We've also noted that the code in sd_diskio.c has the compile time build define "ENABLE_...

LWeir.775 by Associate II
  • 1297 Views
  • 1 replies
  • 0 kudos

Resolved! How to put lis2dw12tr in power down?

Hi im using lis2dw12tr sensor with I2C protocol in my app and i configured sensor in powerdown CTRL1 register i writed 0x00.But i see that on the board on which sensor is placed has current consumption around 370uA. On the board with unmounted sensor...

MKla.1 by Associate III
  • 3428 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.