MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Question about IIS3DWB INTERNAL_FREQ_FINE register

Hello, I’m using the IIS3DWB with an Arduino Portenta, using a procedure similar to Kris Winer’s github (i.e. using the FIFO buffer in continuous mode, 256 watermark, stop on watermark, data ready interrupt on watermark, running various cycles until ...

FCook.1 by Associate III
  • 1026 Views
  • 2 replies
  • 0 kudos

Resolved! consume very high current in lsm6dsox

Hi team,we have configured accelerometer normal mode in the sensorBelow configuration - Accelerometer normal modePower mode - Normal modeG-Range - 16 gODR208HZ CTRL8_XL (0x00) CTRL6_C (0x10) CTRL1_XL (0x54)104 HZ ...

0693W00000F9wNBQAZ.jpg
Sprem.1 by Associate III
  • 2225 Views
  • 3 replies
  • 0 kudos

Resolved! If you could pass your knowledge onto a dev starting their vibration project how would you recommend them to start?

I have spent some time on the forums and can see that there are many options for projects depending on the requirements of the user. I am looking to hear people's opinions on a suitable setup as an introduction to the field. I am a firm believer in w...

HADWLL by Associate
  • 1853 Views
  • 3 replies
  • 0 kudos

Resolved! Is it possible to dinamically change the threshold for the FSM?

Hello,I'm working on a ultra low power application using the LSM6DSO32X. The goal is to have a device that reacts (with a short radio message) when its orientation relative to gravity changes. For this I wish to use as much as possible the FSM and th...

DGiov.1 by Associate III
  • 2155 Views
  • 3 replies
  • 0 kudos

Resolved! Question about LSM6DS3h : why Accel Z value OUTZ_L_XL (2Ch) & (2D) become negative when module acceleration downward but not upside down.

I am using this chip to get the X & Y angle of the unit. First read outOUTX_L_XL (28h) & 29hOUTY_L_XL (2Ah) & 2BhOUTZ_L_XL (2Ch) &2Dhand calculate Roll and Pitch.  The angles works good in normal / slow moving or stable condition. Also need to det...

MLy by Associate II
  • 3313 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.