Lis2dw12 - changing settings without power off the sensor
Is it need to write '1' to SOFT_RESET bit field in CTRL2 register when you change settings for the sensor in CTRL1, CTRL3, CTRL4_INT1_PAD_CTRL, CTRL5_INT2_PAD_CTRL, CTRL6, CTRL7 register ?
Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Is it need to write '1' to SOFT_RESET bit field in CTRL2 register when you change settings for the sensor in CTRL1, CTRL3, CTRL4_INT1_PAD_CTRL, CTRL5_INT2_PAD_CTRL, CTRL6, CTRL7 register ?
I am testing STWINKT1 board, it always use to work without any issues. Off late I am having issues to download the compiled codes into the unit.I connected the unit to ST-LINK Utility , it connects but reports Read out protection is activated.Luckil...
lsm6dsl Step counter - Pedometer. How to get correct data?I get interrupt every small movement detection.My sensor work on 52 HZ I set thresholds and read data(see blow) Thresholds:lsm6dsl_****_debounce_steps_set(&IMU_Ctx, imuParams.debounce_steps); ...
Dear Sir/Madam, I am currently working on the LSM6DSM IMU for a visual-inertial SLAM use and I have some questions about its features. Here is my IMU settings : Gyro : ODR = 208Hz FS = 2000dps High Pass 260mHz Acc : ODR = 208HzFS = 2g Analog BW 400Hz...
i am trying to read the WHO_AM_I (read only) register and transmitting the data ( 0x0F | 0x80 ) and receiving the data from slave (0x6A) while checking in oscilloscope, but here is the problem that when i am driving (MISO) output of slave into mast...
Save the date --- APRIL 28, 2022, SEMI HQThis class will explain and demonstrate how AI/ML logic can be implemented on Edge devices such as Smart sensors. Power efficiency, latency, and bandwidth considerations are important for AI/ML implementation ...
I am getting acceleration and gyro data using LSM6DSO32 chip. But I want to filter this data with internal filters, but I cannot activate the high pass filter of the accelerometer. In the code below, I want to send F4 (11110100) data to the CTRL8_XL ...
Hi, my name is Vincenzo,I'm studying the MotionFX library and I want to understand In what order the quaternion is given by the MotionFX library. Reading the manual, I know that the MotionFX can compute:rotation, quaternions, gravity and linear accel...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.