cancel
Showing results for 
Search instead for 
Did you mean: 

I have NUCLEO-L053R8. Now I need to interface LSM9DS1 directly with NUCLEO-L053R8 for testing using MotionFX Library. Is it possible to interface LSM9DS1 to test using MotionFX library? If Yes, Please suggest proper procedure/steps. Thank you.

VB.4
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Eleon BORLINI
ST Employee

Hi @VB.4,

you can start from the C GIthub examples for the LSM9DS1 device (lsm9ds1_read_data_polling.c), changing the hardware connection for the Vdd / SPI physical lines (from the NUCLEO_F411RE to the NUCLEO-L053R8), and then you can add the MotionFX Library to your project, taking as reference the examples of the X-CUBE-MEMS1 that you can find in the \Projects\STM32L073RZ-Nucleo\Applications\CUSTOM folder.

If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster.

-Eleon

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.