MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I have successfully built AlgoBuilder-based Firmware for my Target: NUCLEO-L476RG + X-NUCLEO-IKS02A1 + ISM330IS In Unicleo GUI, the data is streamed correctly for a few minutes but then stops abruptly. Why?

I put a logic analyzer on the I2C and INT1 line, and note that the INT1 continues to trigger but the I2C lines do not show data transfer anymore. Are there known issues? Is it a problem with the sensor or the host code? It may be dependent on the OD...

JLamb.3 by Associate II
  • 1286 Views
  • 1 replies
  • 0 kudos

Possible bug in Unico GUI v9.13.0.0

Dear ST Community,Have no experience with STM32 MCUs nor with any programming IDEs used to develop for STM chips. As i am developing on espressif MCUs...However recently i am trying to integrate a MEMS sensor of STM into my project.I found out Unico ...

RDyla.1 by Associate
  • 2385 Views
  • 3 replies
  • 0 kudos

The 210/109 combination allows for a register set to select 1666 Hz. If I run the device and do a read only, it may almost run at 1666 Hz, but if you do any real reads and analysis wanting the acceleration, time and frequency the device runs slower

I have about 10 of these devices on about 6 computers, so this problem is common, the device runs at about 1200 to 1400 Hz. The picture shows a temperature, frequency and FFT results plot for one device. The typical is about 1400 +- 50. I take and...

LIS2MDL single shot issues

When running the single shot with offset cancellation mode we will occasionally get the following measurements for the magnetometer:x = -1y = 0 z = -1 temp = -1 This causes issues for us as we are manually averaging the two single shot values togethe...

0693W00000Y7lE5QAJ.png
KPasm.1 by Associate
  • 1115 Views
  • 1 replies
  • 0 kudos

I am interested to use the device to determine the orientation of it in space using lis2dw12 only. As a test, I rotate the device 90 degrees each time over each one of the axes - Roll/Pitch and Yaw as presented in the attached figure.

I get the readings from ax,ay and az(plotted as well).Can the orientation of the lis2dw12 chip be derived from the DC levels? If so - how? What is the purpose of 6D orientation functionality and the accuracy of it?

SPiy.1 by Associate
  • 1241 Views
  • 0 replies
  • 0 kudos

FIFO timestamp (LSM6DSM)

Hi,i was trying to set up the pedometer and timestamp functionality for the FIFO.I was fallowing the instructions on page 102 (chapter 9.1) of the documentation for the setup (high timestamp resolution).It is working on a FIFO ODR of 104Hz. But if i ...

LHeit.1 by Associate II
  • 2088 Views
  • 1 replies
  • 0 kudos

Getting temperature from ISM330IS in AlgoBuilder

I have successfully built AlgoBuilder-based Firmware for my Target, including using some of the ISPU based examples from the x-cube-ispu GitHub:NUCLEO-L476RG + X-NUCLEO-IKS02A1 + ISM330ISWe are hoping to replace an old accelerometer and separate temp...

JLamb.3 by Associate II
  • 2607 Views
  • 3 replies
  • 0 kudos

MotionEC Update Rate

I'm using an LSM303AGR to create a compass using the MotionEC library for calculating quaternions.Since the ODR of the magnetometer inside the LSM303AGR is 20Hz while the ODR of the accelerometer is 25Hz with which frequency and with which data is it...

CSharpino by Associate III
  • 2264 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.