MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Conformal coating - LIS2DW12TR

Hi TeamWe are currently working on ST PN: LIS2DW12TR in our new project. Thus, I would like to check with ST whether this part is OK to be Conformal coated? The reason is, our PCB will need to be conformal coating after all the components are populat...

Resolved! SPI receive the same data every time (it's the register who_am_i)

Hi!I'm using the LaunchPad CC2642R1/CC2652R1 with the accelerometer LIS2DH and i tested the "who am i" (0x33) register to validate the protocol but when i tried read another register i had the same response that "who am i" (0x33) register. Could you ...

0693W00000Y8yEeQAJ.png
TVela.1 by Associate III
  • 2385 Views
  • 9 replies
  • 0 kudos

SensorTile Dev Kit Cradle CPU gets hot

I have recently purchased the SensorTile development kit.I installed/soldered a sensortile and I noticed the LED didnt come on.I then felt the CPU was getting very hot.I reinstalled another sensorTile and the very same thing happened.Note I was extre...

lbbaker by Associate
  • 1924 Views
  • 2 replies
  • 0 kudos

Resolved! LSM6DSR to LSM6DSOX migration issue

We are migrating from LSM6DSR to LSM6DSOX. In LSM6DSR the nominal timestamp resolution used to be around 25 μs. And we used to get 52 samples/sec from the FIFO.However, in LSM6DSOX with a similar setting, we are getting a resolution of around 18 μs. ...

Sachin3 by Associate
  • 1378 Views
  • 1 replies
  • 0 kudos

Resolved! Driver issue on Windows 11

Hello communityI'm having issues with the STEVAL - MKI109V3 board and the Unico GUI. There is no driver identified for the board. I've tried installing the driver for Windows 8, which gets identified but when I try to open Unico GUI, I get an error m...

BVilm.1 by Associate
  • 2750 Views
  • 1 replies
  • 0 kudos

I have just started the: Quick Start Guide Motion MEMS and environmental sensor expansion board for STM32 Nucleo (X-NUCLEO-IKS01A3) And I cant get it work. Unicleo GUI can not recognize the expansion board.

After all installations I cant find my board(NUCLEO-L476RG) in the projects folder.According to example these board are valid:NUCLEO-F401RENUCLEO-L053R8NUCLEO-L152RENUCLEO-L476RGBut these boards could be found:NUCLEO-F401RENUCLEO-L073RZNUCLEO-L152REN...

ABerg.7 by Associate
  • 1607 Views
  • 2 replies
  • 0 kudos

Resolved! LSM6DSO issues with SPI

Hi ST community,Currently we are trying to use the LSM6DSO (6 Axis MEMS sensor) in our project.We were able to successfully test the LSM9DS1 (9 Axis MEMS sensor) using the ST Adapter board STEVAL-MKI159V1 and we had no issues communicating with it an...

KShar.4 by Associate II
  • 16061 Views
  • 14 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.