2023-02-04 9:36 AM
I have about 10 of these devices on about 6 computers, so this problem is common, the device runs at about 1200 to 1400 Hz. The picture shows a temperature, frequency and FFT results plot for one device. The typical is about 1400 +- 50. I take and FFT every 16384 data points, but I have to measure the time for each 16384 data points and adjust the FFT results. I have calibrated it against a standard accelerometer on a known vibration element.
Is this the expected behavoiur? it is not temperature dependent and only windows is running on the devices as they are remote.
I do not mind, I just want to confirm it.
One has to use the ticks on computer clock as the return on the time registers is not accurate enough nor calibrated.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.