MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Selecting a motion sensor

Hi,I am looking for a motion sensor with I2C that can work in the following way:Wake up from low powerStart monitoring acceleration and rotationStop monitoring (about 500ms later)Query most significant motion while monitoringGo back to sleepBasically...

Resolved! LPS22 Device ID

HiI try to read the WHO_AM_I register using SPI but I get 0xB3 instead of 0xB1. Is this correct?Regards

LMatt.5 by Associate
  • 1576 Views
  • 1 replies
  • 0 kudos

LSM6DSMTR Taking more power on VDDIO Pin

I am using LSM6DSMTR  with a coin cell battery. I have connected the IMU with NRF52810 using a SPI line. Attached the screenshot.When I am observing the power profiler, VDDIO is gradually taking current after the SPI communication (I have used a 100...

0693W00000Y9CiiQAF.png 0693W00000Y9CkKQAV.png
V.Jose by Associate II
  • 2023 Views
  • 2 replies
  • 1 kudos

Resolved! LSM6DSLTR device marking

Hi!Our incoming inspection unit failed to find any information on LSM6DSLTR device marking. We got parts with 2 lines on it.SF2D code106 Could you please confirm it is a LSM6DSLTR device? Is there date code on it?

0693W00000aHDY5QAO.png
AAGree by Associate II
  • 3248 Views
  • 3 replies
  • 0 kudos

Reading temperature from the LSM303AGR.

I am initializing the 303 with the following code: /* Turn on accelerometer */ WriteRegister(LSM303AGR_CTRL_REG1_A, LSM303AGR_ADDR_WRITE_A, 0x57); x = ReadRegister(LSM303AGR_CTRL_REG1_A, LSM303AGR_ADDR_READ_A);   /* Turn on temp sensor and set BDU bi...

BMart.2 by Associate II
  • 4180 Views
  • 6 replies
  • 0 kudos

STM32F4 i2c vs LSM303DLHC i2c

Trying to match STM32F4 with LSM303DLHC and I cannot find for i2c addressing mode of type: Master: | ST | SAD + W | SAK | SUB | SAK | SR | SAD + R | SAK | ... any match in the STN32F4 7 or 10 bit addressing modes. I suppose using all those bits it is...

ACht.1 by Associate
  • 1519 Views
  • 3 replies
  • 0 kudos

Resolved! LPS22HB SPI interface

HiHas nobody used the sensor using SPI interface? I have a power up issue, if CS is left floating till processor drive it to zero it seems device start as i2C and micro Dout is shorted to ground.

LMatt.4 by Associate
  • 2002 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.