2023-02-15 1:55 PM
Hi,
I am looking for a motion sensor with I2C that can work in the following way:
Basically the MCU will wake up the sensor, reset it's memory and then do other things (like reading other sensors..) and when done, about 500ms later, ask the sensor what was the most significant motion change during this time.
I read a few datasheet, and found some sensors with a FIFO, like the LSM6DSO, but it would require reading all data and do the aggregation on the MCU.
I would really love a chip that can provide a single "summary" of the motion.
It is important to have small sleep power consumption, but it seems they are all in the uA range, so it is good enough.
2023-02-21 3:13 AM
I found the ISM330IS which would allow me to write a firmware, I guess that would work, but I am wondering if a simpler solution exists.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.