MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

What's the data latency and g-sensitivity for LSM6DSO32?

Hi!Me and my team are currently working on project which include LSM6DSO32 sensor. There's two parameters that don't seem to be listed in datasheet or application note:1) Data latency [ms] - time between the moment the sensors are sampled and the mom...

RNawr.1 by Associate
  • 1494 Views
  • 1 replies
  • 1 kudos

step counter detection not working on lsm6dsr

Enabling "step counter detection" on lsm6dsr using the application note [1] "basic SW routine" does not seem to work (1-13 routine steps). Device always reads the value: 2C00h from registers 62h and 63h. Any pointers on how to debug the issue?[1]: ht...

AHuta.1 by Associate
  • 1413 Views
  • 1 replies
  • 0 kudos

How to configure S4S sensor synchronization in LSM6DSRX module

The iNEMO inertial module LSM6DSRX supports sensor synchronization S4S for Qualcomm. Sensor data sheet mentions following S4S registers without much detail.S4S_TPH_L (04h) Sensor synchronization time frame register - low byte (r/w)S4S_TPH_H (05h) S...

farid by Associate II
  • 2435 Views
  • 1 replies
  • 0 kudos

Resolved! LIS3DHTR Product Life cycle?

Hi,In the company where I work we are developing hardware and we are already evaluating the LIS3DH in order to put it in our hardware devices. However we have noticed that the LIS3DH is obsolete but there is the LIS3DHTR which is the same product but...

VGuer by Associate II
  • 6445 Views
  • 11 replies
  • 0 kudos

LIS2DH12TR- Not working on 2.9V and above voltages

Hello,I am using LIS2DH12TR through SPI but I am not able to operate it on greater than 2.8V. On greater than 2.8V I am not able to read the device ID. But according to the datasheet, it is able to operate up to 3.6 V. SO how can I use this ic greate...

Smalik by Associate II
  • 8449 Views
  • 22 replies
  • 0 kudos

Resolved! [STPM3x] Production date ?

Hi,I have a STPM33 on some of my PCB and I have issue with some of them when it gets too hot. The actual datasheet tells us that the operating temperature range is -40C to +105C but I've found an old one of October 2013, another of October 2014, anot...

carton by Associate II
  • 2245 Views
  • 3 replies
  • 0 kudos

Resolved! MEMS SMD device marking "SO"

Hi, can anybody tell me what partnumber this is. The chip is a LGA-14 package with the "SO" marking. It is probably an accelerometer.I aslo tried to read the 2d matrix code and it says: 781120R903QE

WVleu.1 by Associate II
  • 4101 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.