MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Is license needed to use MotionAC libraries

Hi,I am working on project using ZephyrOS and I am trying to link in and use some of your motion libraries.I have successfully linked but the call to MotionAC_GetLibVersion() is returning zero. Looking at assember in my debugger a variable is being t...

capacitive touch with brass metal

Hi,I want to design a capacitive touch application with a brass metal plate. So, i need a sensor that is suitable with brass metal. Is there any advised product for me?

er3481 by Senior
  • 1404 Views
  • 1 replies
  • 0 kudos

SAI1_SD_A Pin Change Issue in Project BVLINKWB1 V2.0.0

Hi All,I am using a P-NUCLEO-WB55 development board in BVLINKWB1_V2.0.0 project. Project ST Link Here: https://www.st.com/en/embedded-software/fp-aud-bvlinkwb1.htmlIn this project, I would like to change the SAI1_SD_PIN from PA10 to PB15 in P-NUCLEO-...

0_PA10_Successfull_Test.png 2_Noisy_Changed_PB15_Pin.png Default_Alternate_Functions.png Desired_Alternate_Functions.png

Configuration wrong and calibration wrong for ISM330DLC

Hello I'm acquiring data from an ISM330DLC per I2C, and I'm having several issues:-I probably have the config wrong several levels. For instance I have the Reg CTRL1_XL configured to 0x75, CTRL2_XL to 0x7C, CTRL8_XL to C8, CTRL7_G to 40, CTRL6_C to 0...

IIS3DWB temperature sensor offset

HelloIn the IIS3DWB datasheet, it is said that the embeddeed temperature sensor offset can vary within a [-15°C : +15°C] range.Does that mean that the reading from OUT_TEMP_H/L can vary within [-256*15 LSB : +256*15 LSB] at 25°C ?Having tested 2 chip...

pb38 by Associate II
  • 7442 Views
  • 12 replies
  • 0 kudos

Resolved! LSM6DSR is never setting XLDA in status reg.

I am trying to validate a new board layout and am looking for the minimal configuration to read accel data.I'm using SPI.  When the WHO_AM_I register of the LSM6DSR is queried, the correct response of 0x6B is returned.I take that as validation of the...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.