MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! What do the self-tests of the ASM330LHH actually prove?

Hello, I hope you are well.I had a query about the IMU ASM330LHH. I want to know whether the self-test functions of the internal accelerometer and gyroscope (see attached pictures) test the internal MEMS sensors or not. I have doubts whether these se...

FedIng by Associate
  • 3989 Views
  • 2 replies
  • 2 kudos

ISM330DHCX: accelerometer usable bandwidth

Hi, at my parttime job we are using the ISM330DHCX in an industrial sensor for measuring acceleration, gyro and inclination. In the description for ISM330DHCX is stated, that it can be also used for vibration measuring. In the datasheet (p.50/167 Tab...

APozd.2 by Associate
  • 2931 Views
  • 2 replies
  • 0 kudos

Audio USB interface for IM69D130 MEMS Microphones

I recently bumped into an audio USB interface which might fits my needs : the STEVAL-MKI138V1. Indeed, I want to get the audio signals of 4 MEMS IM69D130 microphones onto my PC on Audacity, through a USB audio interface like the STEVAL-MKI138V1. Howe...

Do IMP23ABSU have only MEMS transducer or with any amplifier?

Hello, I want to find some MEMS transducer for microphone for testing our readout IC for MEMS microphone No matter with single or differential output, but the product that I need is the transducer without input buffer, output amplifier and other. Is ...

JKim.38 by Associate
  • 1033 Views
  • 0 replies
  • 0 kudos

Resolved! Where to download Unicleo-GUI?

Hello,I have found informations about Unicleo-GUI, and I would like to test it. There are many informations on ST page, but I could not find any link to download it.So where can I download it?Thank you

ANauz.1 by Senior II
  • 3717 Views
  • 5 replies
  • 0 kudos

Resolved! Cannot make accelerometer LIS2DU12 in Sensor.Tile Pro working ?

Hello, I cannot make the LIS2DU12 working in the Sensor.Tile module. I followed the instruction in the AN5648 but I get random values for X, Y, Z. At first, I'm trying to get the readings in normal continuous mode without FIFO. I can connect the devi...

jea74 by Associate III
  • 1923 Views
  • 1 replies
  • 0 kudos

using STEVAL-MKI221V1 adaptor on STEVAL-MKI109V2

Hey, I wanna use MKI221V on MKI109V2, the sensor datasheet says that it's - "Compatible with STEVAL-MKI109V2 by changing resistor settings". Couldn't find any references to what resistor settings are needed and how to implement them, any help would b...

Lev_G by Associate
  • 1137 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.