2023-09-26 12:57 AM
I set the CTRL1_XL (10h) of ISM330ISN as 0xA4 ,so the ODR of ISM330 is 6667Hz.
If I want transmit the whole data @6667Hz to external RS485 ,How tocontroll it ?
Can I Using the ISM330 INT1 to trigger every transaction ? or independently transmit data using timer of
STM32L431CCT6?
2023-09-26 8:04 AM
Hi @JohnGe ,
Welcome to ST Community!
I would suggest to send more data with a single communication, so the best way would be to use the FIFO, save a certain number of data and then send every data with a single UART communication. As an easier version, you could also try to use the normal interrupt and use a custom FIFO inside your code where you store all the data and then send it in a single comm every once in a while.
If this helps you, please mark my answer as "Best Answer" by clicking on the "Accept as Solution" button, this can be helpful for Community users to find this solution faster.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.