MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS2DE12 - Sleep to Wake Function

Hello,I'm looking to see if there is a maximum value for the sleep-to-wake interrupt register on the LIS2DE12. I do see +/- 2g, 4g, 8g, 16g as standard values, but is it okay to set a threshold value to +/-30g, 25g or 20g?Thanks!

Resolved! LIS3MDL set/reset circuit

Hi,We were looking at the LIS3MDL sensor. Apparently it is a magnetoresistive sensor. When we examined other magnetoresistive sensors in the market we have seen that they need set/reset circuits in order to compensate for the disturbances in the magn...

Q&A - Instagram live event on SensorTile.box PRO

What are the typical applications of the SensorTile.box PRO? The Sensortile.box PRO is a programmable wireless box kit that can be used in IoT applications based on remote data gathering and evaluation. Examples are smart home devices, healthcare, sm...

LSM6DSO different versions, from new batch does not work

Hey, We are using LSM6DSO in our Smart Bear to wake up the electronics when the Bear is moved. Now with the new electronics card having a LSM6DSO from a different batch does not work with the same Firmware and circuit design. Previously LSM6DSO was f...

DFSDM Filter for DC-Bias of MEMS-MIC

Hello st-community,I am currently working with MEMS microphones (more precisely: MP34DT05TR-A). For reading in the data I use the DFSDM, which also works as far as possible, because I noticed when evaluating the data using an FFT that there is a very...

spectrum.PNG
ChRegBrg by Associate II
  • 1633 Views
  • 1 replies
  • 0 kudos

Resolved! LSM6DSV16BX Bone conduction feature

I used LSM6DSV16BX for bone conduction detection. Based on the sample code and driver provided on github, everything related to the I2C works fine. But when it comes to the TDM part, I can not get any valid data from the tdm port.my platform is esp32...

Ayse by Associate
  • 3340 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.